cancel
Showing results for 
Search instead for 
Did you mean: 

USBX Device MSC in Standalone mode in STM32u083

naveenkumar-192
Associate II

I am trying to get USBX Device MSC to work in Standalone mode (without RTOS) on Stm32u083mc microcontroller. However, I am interested in configuring an external Flash as a mass storage device. i am using the same clock frequency of HID standalone example which i referred from official STM32U0 Work shop tutorial from youtube. Now i am planning for mass storage class, i am defining pool_size and stack_size is from app_usbx_device.h file 

#define UX_DEVICE_APP_MEM_POOL_SIZE (10*1024)

#define USBX_DEVICE_MEMORY_STACK_SIZE (10*1024).
from MX_USBX_Device_Init() function i am getting usbd_ok. before returing i am calling these function USBX_APP_Device_Init();

VOID USBX_APP_Device_Init(VOID)

{

MX_USB_PCD_Init();

 

// Endpoint 0 (Control)

HAL_PCDEx_PMAConfig(&hpcd_USB_DRD_FS, 0x00, PCD_SNG_BUF, 0x00); // EP0 OUT at PMA offset 0x00

HAL_PCDEx_PMAConfig(&hpcd_USB_DRD_FS, 0x80, PCD_SNG_BUF, 0x40); // EP0 IN at PMA offset 0x40

 

// Endpoint 1 (MSC Bulk)

HAL_PCDEx_PMAConfig(&hpcd_USB_DRD_FS, 0x01, PCD_SNG_BUF, 0x80); // EP1 OUT at PMA offset 0x80

HAL_PCDEx_PMAConfig(&hpcd_USB_DRD_FS, 0x81, PCD_SNG_BUF, 0xC0); // EP1 IN at PMA offset 0xC0

 

ux_dcd_stm32_initialize((ULONG)&hpcd_USB_DRD_FS, (ULONG)&hpcd_USB_DRD_FS);

 

HAL_PCD_Start(&hpcd_USB_DRD_FS);

}

UINT MX_USBX_Device_Init(VOID)

{

UINT ret = UX_SUCCESS;

UCHAR *device_framework_high_speed;

UCHAR *device_framework_full_speed;

ULONG device_framework_hs_length;

ULONG device_framework_fs_length;

ULONG string_framework_length;

ULONG language_id_framework_length;

UCHAR *string_framework;

UCHAR *language_id_framework;

 

UCHAR *pointer;

 

/* USER CODE BEGIN MX_USBX_Device_Init0 */

 

/* USER CODE END MX_USBX_Device_Init0 */

pointer = ux_device_byte_pool_buffer;

 

/* Initialize USBX Memory */

if (ux_system_initialize(pointer, USBX_DEVICE_MEMORY_STACK_SIZE, UX_NULL, 0) != UX_SUCCESS)

{

/* USER CODE BEGIN USBX_SYSTEM_INITIALIZE_ERROR */

 

return UX_ERROR;

/* USER CODE END USBX_SYSTEM_INITIALIZE_ERROR */

}

 

/* Get Device Framework High Speed and get the length */

device_framework_high_speed = USBD_Get_Device_Framework_Speed(USBD_HIGH_SPEED,

&device_framework_hs_length);

 

/* Get Device Framework Full Speed and get the length */

device_framework_full_speed = USBD_Get_Device_Framework_Speed(USBD_FULL_SPEED,

&device_framework_fs_length);

 

/* Get String Framework and get the length */

string_framework = USBD_Get_String_Framework(&string_framework_length);

 

/* Get Language Id Framework and get the length */

language_id_framework = USBD_Get_Language_Id_Framework(&language_id_framework_length);

 

/* Install the device portion of USBX */

if (ux_device_stack_initialize(device_framework_high_speed,

device_framework_hs_length,

device_framework_full_speed,

device_framework_fs_length,

string_framework,

string_framework_length,

language_id_framework,

language_id_framework_length,

USBD_ChangeFunction) != UX_SUCCESS)

{

/* USER CODE BEGIN USBX_DEVICE_INITIALIZE_ERROR */

 

return UX_ERROR;

/* USER CODE END USBX_DEVICE_INITIALIZE_ERROR */

}

 

/* Initialize the storage class parameters for the device */

storage_parameter.ux_slave_class_storage_instance_activate = USBD_STORAGE_Activate;

storage_parameter.ux_slave_class_storage_instance_deactivate = USBD_STORAGE_Deactivate;

 

/* Store the number of LUN in this device storage instance */

storage_parameter.ux_slave_class_storage_parameter_number_lun = STORAGE_NUMBER_LUN;

 

/* Initialize the storage class parameters for reading/writing to the Flash Disk */

storage_parameter.ux_slave_class_storage_parameter_lun[0].

ux_slave_class_storage_media_last_lba = USBD_STORAGE_GetMediaLastLba();

 

storage_parameter.ux_slave_class_storage_parameter_lun[0].

ux_slave_class_storage_media_block_length = USBD_STORAGE_GetMediaBlocklength();

 

storage_parameter.ux_slave_class_storage_parameter_lun[0].

ux_slave_class_storage_media_type = 0;

 

storage_parameter.ux_slave_class_storage_parameter_lun[0].

ux_slave_class_storage_media_removable_flag = STORAGE_REMOVABLE_FLAG;

 

storage_parameter.ux_slave_class_storage_parameter_lun[0].

ux_slave_class_storage_media_read_only_flag = STORAGE_READ_ONLY;

 

storage_parameter.ux_slave_class_storage_parameter_lun[0].

ux_slave_class_storage_media_read = USBD_STORAGE_Read;

 

storage_parameter.ux_slave_class_storage_parameter_lun[0].

ux_slave_class_storage_media_write = USBD_STORAGE_Write;

 

storage_parameter.ux_slave_class_storage_parameter_lun[0].

ux_slave_class_storage_media_flush = USBD_STORAGE_Flush;

 

storage_parameter.ux_slave_class_storage_parameter_lun[0].

ux_slave_class_storage_media_status = USBD_STORAGE_Status;

 

storage_parameter.ux_slave_class_storage_parameter_lun[0].

ux_slave_class_storage_media_notification = USBD_STORAGE_Notification;

 

/* USER CODE BEGIN STORAGE_PARAMETER */

 

/* USER CODE END STORAGE_PARAMETER */

 

/* Get storage configuration number */

storage_configuration_number = USBD_Get_Configuration_Number(CLASS_TYPE_MSC, 0);

 

/* Find storage interface number */

storage_interface_number = USBD_Get_Interface_Number(CLASS_TYPE_MSC, 0);

 

/* Initialize the device storage class */

if (ux_device_stack_class_register(_ux_system_slave_class_storage_name,

ux_device_class_storage_entry,

storage_configuration_number,

storage_interface_number,

&storage_parameter) != UX_SUCCESS)

{

/* USER CODE BEGIN USBX_DEVICE_STORAGE_REGISTER_ERROR */

 

 

return UX_ERROR;

/* USER CODE END USBX_DEVICE_STORAGE_REGISTER_ERROR */

}

 

/* USER CODE BEGIN MX_USBX_Device_Init1 */

 

 

USBX_APP_Device_Init();

/* USER CODE END MX_USBX_Device_Init1 */

 

return ret;

}

i am using heap and stack is

_Min_Heap_Size = 0x200; /* required amount of heap */

_Min_Stack_Size = 0x400; /* required amount of stack */

 

I am not sure what might be the issue, but i tried calling ux_device_stacks_run(); in while at the time it was enetring into Hardfault error

 

but even though i am getting popup like USB Device is not recognized.

4 REPLIES 4
Saket_Om
ST Employee

Hello @naveenkumar-192 

Please refer to the example below:

STM32CubeU5/Projects/STM32U575I-EV/Applications/USBX/Ux_Device_MSC at main · STMicroelectronics/STM32CubeU5 · GitHub

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Saket_Om
FBL
ST Employee

Hi @naveenkumar-192 

First, are you using a reference board? U083 DK?

I recommend increasing your stack and heap sizes. 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL

Hii @FBL yeah i am using STM32U083C-DK, i am using heap size and stack size _Min_Heap_Size = 0x200; _Min_Stack_Size = 0x400;  and i am using clock source for usb is HSI 48MHz, in RCC configuration i am using CRS SYNC Source USB for main clock i am not using HSE, HSI, i am using MSI 48000KHz. I am trying  Mass storage class in Standalone.

Hi @Saket_Om @FBL I already referred above example, but i am trying for External flash memory(w25q64jv) or i am trying to implement some ram portion as mass storage is that possible?. If possible can i get applications notes for usbx. i am facing the issue like device is not recognized.