2024-12-18 8:07 AM
I'm trying to establish a TCP connection between my Nucleo-H753ZI and my PC.
I'm using ThreadX and NetxDuo.
First of all, i'm triggering a hard fault when activating Network Interfaces and then using the debug mode.
I don't seem to have hard fault if i flash the program directly into the board (I have a thread that blinks an LED that still works)
This is my cubeMX configuration :
I installed the following, using the Software Packs Component Selector:
STMicroelectronics-X-CUBE-AZRTOS-H7:
ThreadX => Core
NetXDuo => NX Core
Network Interfaces => Ethernet Interface, Ethernet Phy Interface : LAN8742_Phy_Interface
Board Part STM32Cube_BSP_Components : ETHPhy / LAN8742
I tried to ping the board using CMD in windows, but i'm guessting that wouldn't work because i haven't added any code in nx_app_thread_entry.
Thank you
2024-12-18 8:09 AM - last edited on 2024-12-18 8:12 AM by Andrew Neil
Duplicate post - merged
I'm trying to establish a TCP connection between my Nucleo-H753ZI and my PC.
I'm using ThreadX and NetxDuo.
First of all, i'm triggering a hard fault when activating Network Interfaces and then using the debug mode.
I don't seem to have hard fault if i flash the program directly into the board (I have a thread that blinks an LED that still works)
This is my cubeMX configuration :
I installed the following, using the Software Packs Component Selector:
STMicroelectronics-X-CUBE-AZRTOS-H7:
ThreadX => Core
NetXDuo => NX Core
Network Interfaces => Ethernet Interface, Ethernet Phy Interface : LAN8742_Phy_Interface
Board Part STM32Cube_BSP_Components : ETHPhy / LAN8742
I tried to ping the board using CMD in windows, but i'm guessting that wouldn't work because i haven't added any code in nx_app_thread_entry.
Thank you
2024-12-18 8:11 AM - edited 2024-12-18 10:08 AM
On debugging Hard Faults - both Cortex-M in general, and STM32 specifically:
@unkn0wn wrote:I'm using ThreadX and NetxDuo.
Presumably they can provide some diagnostic tracing to (help) see what's going on ?
You can, of course, add your own ...
PS:
NetXDuo Knowledge Base articles:
2024-12-18 10:05 AM
Hi @unkn0wn ,
First of all please make sure that your Ethernet buffers are not in AXI SRAM as Ethernet MAC has no access to it.
Regards,
Dmitry
2024-12-19 9:08 AM
Hi @DmitryR
Actually, the Ethernet MAC has access to AXI SRAM as shown below in the bus matrix.
the only unaccessible memory is the DTCM.
regards
haithem.
2024-12-20 2:21 AM
@Haitem,
First of all you show the picture for the H723 but @unkn0wn uses H753. For H753, this link from Ethernet MAC to AXI bridge was added in documentation revision 10 only. I do not know the reason but I know that for silicon revisions Y and V this does not work, I have had this problem myself. Putting Ethernet buffers to AHB SRAM makes it work without any problems.
Regards,
Dmitry
2024-12-20 5:31 AM
Sorry @DmitryR
Indeed I used the wrong reference manual, here is the correct one to keep the tracking.