2024-09-26 9:02 AM
Hi,
I am still trying to intetrage my custom board with an STM32WB55CG into my Tuya/Smartlife System with the target of transmitting sensordata and receiving commands (e.g. LED color).
In this https://community.st.com/t5/stm32-mcus-wireless/stm32wb55cg-zigbee-connection-tuya-smartlife-with-st-example/m-p/720530#M21149 question, I was told to use P-NUCLEO-WB55.Nucleo\Applications\Zigbee\Zigbee_OnOff_Client_Distrib Example with which I could successfully connect the controller to my network.
Since I have a custom board (other chip than Nucleo), I needed to create a new CubeMX project in which I copied all interfaces from the example and applied my pinout.
In CubeMX I found the option to configure my Chip to a Zigbee purpose already, so I chose the following settings:
| Setting | My Project | Example |
| Zigbee Application | Full Function Device | Full Function Device |
| Zigbee Network Mode | Centralized | Distributed |
| Zigbee Device Role | Router | N/A |
| HWUART | Disabled | Enabled |
| Device ID | OnOff Switch | OnOff Switch |
Unfortunately I could not get the same result with my custom project. Furthermore, now I have access to UART and tried to output the debug messages, and therefore found out that the init function from "app_zigbee.c" is never even called.
Since some of the settings are different, I tried copying the complete content from Example "app_zigbee.c" and "app_entry.c" to my project, the result is still the same.
I expected, that now everything should be the same an I will be able to connect the device again. For the case that I missed something in the configuration, I attached my CubeMX file. I can also share the project if needed.
Thanks for your help
Solved! Go to Solution.
2024-09-27 2:22 AM
Hello,
It seems that the IPCC interrupts are note activated on your IOC file making the communication impossible between M0/M4, the app_zigbee_init will not be called in this case.
Please activate the IPCC Tx and Rx interrupts as follow and give it a try :
Best regards,
Ouadi
2024-09-27 2:22 AM
Hello,
It seems that the IPCC interrupts are note activated on your IOC file making the communication impossible between M0/M4, the app_zigbee_init will not be called in this case.
Please activate the IPCC Tx and Rx interrupts as follow and give it a try :
Best regards,
Ouadi
2024-09-29 5:57 AM
Hi Ouadi,
thank you very much, I manged to get it running thanks to your help. For other use cases (temperature sensor, LED control), I came across the same problem with Tuya/Smartlife as here https://community.st.com/t5/stm32-mcus-wireless/stm32wb5mm-dk-connecting-to-tuya-gateway-with-zigbee-part-2/m-p/630003 . My plan is now, to create a Zigbee2mqtt and Homeassistent Network and hope, that the problem is not valid there.
Additionally, my MCU can not automatically reconnect to the network after restart. I have seen from here https://community.st.com/t5/stm32-mcus-wireless/rejoining-zigbee-network-fails/td-p/640696 that there are NVM examples available. I have two questions regarding that:
Thanks
2024-09-30 1:37 AM
Hi @vh789,
Good to hear that your issue is now solved.
Please find below my answers :
For any other question, please raise a new post.
Regards,
Ouadi