2022-10-28 03:42 AM
Hello together
Actual I use the systembootloader to update the device over uart.
Is there a way to reconfigure the unused I/O pin for the system bootloader? Or must this be done via a self-written bootloader?
The problem is that some I/O pins take on a different status as soon as the application for the firmware update jumps into the system bootloader.
Thank you and br
2022-10-28 07:18 AM
Systembootloader can be used only with pins defined in AN2606