cancel
Showing results for 
Search instead for 
Did you mean: 

filex and directory/files

IVent.1
Senior

Hallo, this is my code.

I create a directory, and then a file in this directory. If, in another point of the code, I check if the file is present or not, I can read/write it correctly and so on.

Instead, if I stop the execution of the program, when I restart it, I don't find the file above, only the directory.

Any suggestion please? I'm struggling with it...

fxRes = fx_media_open( &disk1, "FS", fx_stm32_levelx_nor_driver, (VOID *)LX_NOR_OSPI_DRIVER_ID, (VOID *) fx_nor_ospi_media_memory, sizeof(fx_nor_ospi_media_memory)); if (FX_SUCCESS != fxRes) { return; } if (!FolderExists(&disk1, (char*)"/DATA")) { fxRes=_fx_directory_create(&disk1, (char*)"/DATA"); if (FX_SUCCESS != fxRes) { return; } } if (!FileExists(&disk1, (char*)"/DATA/file.txt")) { fxRes=_fx_file_create(&disk1, (char*)"/DATA/file.txt"); if (FX_SUCCESS != fxRes) { return; } } fx_media_flush(&disk1); fx_media_close(&disk1);
View more
6 REPLIES 6
mÆŽALLEm
ST Employee

Hello @IVent.1 ,

Please kindly use </>  button to paste your code. I've edited your post then.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
MFARH.1
ST Employee

 To resolve this issue, we need to ensure that we correctly test the FX_ALREADY_CREATED condition when creating directories and files.

 
fxRes = fx_media_open(&disk1, "FS", fx_stm32_levelx_nor_driver, (VOID *)LX_NOR_OSPI_DRIVER_ID, (VOID *) fx_nor_ospi_media_memory, sizeof(fx_nor_ospi_media_memory)); if (FX_SUCCESS != fxRes) { return; } fxRes=_fx_directory_create(&disk1, (char*)"/DATA"); if (FX_SUCCESS != fxRes) { if (FX_ALREADY_CREATED != fxRes) { return; } } fxRes=_fx_file_create(&disk1, (char*)"/DATA/file.txt"); if (FX_SUCCESS != fxRes) { if (FX_ALREADY_CREATED != fxRes) { retrun; } } fx_media_flush(&disk1); fx_media_close(&disk1);
View more
<fxRes=_fx_directory_create(&disk1, (char*)"/DATA");

if (FX_SUCCESS != fxRes)
{
    if (FX_ALREADY_CREATED != fxRes)
    {
      return;
    }
}

fxRes=_fx_file_create(&disk1, (char*)"/DATA/file.txt");

if (FX_SUCCESS != fxRes)
{
   if (FX_ALREADY_CREATED != fxRes)
   {
       retrun;
   }

}>
these 2 _fx_file_create result successfully.
But if I switch off and then on the board, the file created inside the directory is not present anymore.
This is my issue.

Could you please tell me which version of the FileX middleware you are currently using?

<

#define FILEX_MAJOR_VERSION 6

#define FILEX_MINOR_VERSION 2

#define FILEX_PATCH_VERSION 0

>

I conducted an exercise on the B-U585I-IOT02A board using FileX middleware version 6.2.0.

The exercise involved creating a directory and then a file within that directory. The file is correctly written and read in the directory.

However, if I switch the board off and then on again, the file created inside the directory remains present.