2020-06-25 1:35 AM
Hello,
I've checked multiple threads on FATfs design for SPI flash. I see, there are some advantages of using FATfs like standard code, modularity etc. but are there any disadvantages apart from adding one more layer of execution between application and physical layer.
I want to reserve 2MB memory for code file(this is the section which will be used in boot loader code for firmware update) will it be possible if I use file system method.
Thanks,