2016-11-26 6:51 PM
2016-11-27 8:35 AM
Nucleo L476RG here.
Cube, and HAL libraries are the NEW THING. They are obviously, to the unsuspecting new folks that have tried several examples and applications, NOT tested to all degrees in all IDE environments. And ''EX'' appear to = AFTERTHOUGHT.Middleware being so far the worst time consumer.
Yes frustrating.2016-12-08 12:05 AM
Hi.
Either run the example from the folder, or follow this training:
Good luck.
2016-12-08 11:14 AM
Also, With Truestudio, I have found you can run into path length problems if he Project files are more than 7 or so levels down in the directory structure. I usually always put the Cube projects at the root. When they unzip they are in a Stm32L something or other folder so it doesn't splatter files all over the root directory. I hate it when that happens.... :\
Hopefully you found success with it.
2016-12-08 11:48 AM
The problem is i am using Imagecraft C compiler and IDE which is based on CodeBlocks.
I did download TS and have used it. It works great and integrated with MX, but i like Imagecraft.
I can build programs using LL drivers but not the hal drivers, one of the problems is it looks for the compiler used
in cmo.h file which imagecraft is not there : )
TS is good but a bit overkill. I really like simple. TS is kind of slow compiling and really slow downloading via the
STLink.
Thank you for responding. Isnt this forum much BETTER !
2016-12-08 1:06 PM
Yeah IDE's abound. Stick with what you know/like. I had to grab new completely (to me) since my TOOLMANAGER and HEW IDE's (Renesas) were pretty much useless to the Arm world parts. Coming into TS from those is an eye opener....
Compiles and downloads like lightening for me . Plus feature rich comparative to my past.
And you're very welcome.
'Isnt this forum much BETTER !'
Without a doubt! Much MUCH better. But for some d a r n reason my DELETE key quits working on here at odd times and that is ODD.....Doesn't ever do it anywhere except this forum.
2016-12-09 12:29 AM
Hello
Palmer.Randall
,If you have any issue, question or feedback about this community, go to 'About this community' to ask our community team. They can help you.
Best Regards
-Imen-