cancel
Showing results for 
Search instead for 
Did you mean: 

ethernet interrupt not working

root437
Associate II

I send an ethernet packet to MAC address 00:80:E1:00:00:00 but no interrupt occurs in STM

Enabled Ethernet interrupts in CubeMX.

What could be wrong?

Code:

/* USER CODE BEGIN Header */
/**
  ******************************************************************************
  * @file           : main.c
  * @brief          : Main program body
  ******************************************************************************
  * @attention
  *
  * Copyright (c) 2023 STMicroelectronics.
  * All rights reserved.
  *
  * This software is licensed under terms that can be found in the LICENSE file
  * in the root directory of this software component.
  * If no LICENSE file comes with this software, it is provided AS-IS.
  *
  ******************************************************************************
  */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "string.h"
 
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
 
/* USER CODE END Includes */
 
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
 
/* USER CODE END PTD */
 
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
 
/* USER CODE END PD */
 
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
 
/* USER CODE END PM */
 
/* Private variables ---------------------------------------------------------*/
#if defined ( __ICCARM__ ) /*!< IAR Compiler */
#pragma location=0x30000000
ETH_DMADescTypeDef  DMARxDscrTab[ETH_RX_DESC_CNT]; /* Ethernet Rx DMA Descriptors */
#pragma location=0x30000200
ETH_DMADescTypeDef  DMATxDscrTab[ETH_TX_DESC_CNT]; /* Ethernet Tx DMA Descriptors */
 
#elif defined ( __CC_ARM )  /* MDK ARM Compiler */
 
__attribute__((at(0x30000000))) ETH_DMADescTypeDef  DMARxDscrTab[ETH_RX_DESC_CNT]; /* Ethernet Rx DMA Descriptors */
__attribute__((at(0x30000200))) ETH_DMADescTypeDef  DMATxDscrTab[ETH_TX_DESC_CNT]; /* Ethernet Tx DMA Descriptors */
 
#elif defined ( __GNUC__ ) /* GNU Compiler */
ETH_DMADescTypeDef DMARxDscrTab[ETH_RX_DESC_CNT] __attribute__((section(".RxDecripSection"))); /* Ethernet Rx DMA Descriptors */
ETH_DMADescTypeDef DMATxDscrTab[ETH_TX_DESC_CNT] __attribute__((section(".TxDecripSection")));   /* Ethernet Tx DMA Descriptors */
 
#endif
 
ETH_TxPacketConfig TxConfig;
 
ETH_HandleTypeDef heth;
 
/* USER CODE BEGIN PV */
 
int flag = 0;
ETH_MACFilterConfigTypeDef 	macfilter;
uint8_t 		   rxBuffer[152028] = {0};
 
unsigned char txbuf[256+14];
ETH_TxDescListTypeDef  * txdesc;
 
unsigned char rxbuf[256+14] ={0};
ETH_DMADescTypeDef rxdesc;
 
 
  ETH_BufferTypeDef txBuffer;
/* USER CODE END PV */
 
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MPU_Config(void);
static void MX_GPIO_Init(void);
static void MX_ETH_Init(void);
/* USER CODE BEGIN PFP */
 
/* USER CODE END PFP */
 
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
 
/* USER CODE END 0 */
 
/**
  * @brief  The application entry point.
  * @retval int
  */
int main(void)
{
  /* USER CODE BEGIN 1 */
 
  /* USER CODE END 1 */
 
  /* MPU Configuration--------------------------------------------------------*/
  MPU_Config();
 
  /* MCU Configuration--------------------------------------------------------*/
 
  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();
 
  /* USER CODE BEGIN Init */
 
  /* USER CODE END Init */
 
  /* Configure the system clock */
  SystemClock_Config();
 
  /* USER CODE BEGIN SysInit */
 
  /* USER CODE END SysInit */
 
  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_ETH_Init();
  /* USER CODE BEGIN 2 */
 
  /* USER CODE END 2 */
 
  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {
 
	  if (flag == 1)
	  		  {
	  		  flag = 0;
	  		  }
	  	  HAL_Delay(1000);
    /* USER CODE END WHILE */
 
    /* USER CODE BEGIN 3 */
  }
  /* USER CODE END 3 */
}
 
/**
  * @brief System Clock Configuration
  * @retval None
  */
void SystemClock_Config(void)
{
  RCC_OscInitTypeDef RCC_OscInitStruct = {0};
  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 
  /** Supply configuration update enable
  */
  HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);
 
  /** Configure the main internal regulator output voltage
  */
  __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);
 
  while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
 
  /** Initializes the RCC Oscillators according to the specified parameters
  * in the RCC_OscInitTypeDef structure.
  */
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
  RCC_OscInitStruct.HSIState = RCC_HSI_DIV1;
  RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    Error_Handler();
  }
 
  /** Initializes the CPU, AHB and APB buses clocks
  */
  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                              |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
                              |RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
  RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV1;
  RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV1;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV1;
  RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV1;
  RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV1;
 
  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
  {
    Error_Handler();
  }
}
 
/**
  * @brief ETH Initialization Function
  * @param None
  * @retval None
  */
static void MX_ETH_Init(void)
{
 
  /* USER CODE BEGIN ETH_Init 0 */
 
  /* USER CODE END ETH_Init 0 */
 
   static uint8_t MACAddr[6];
 
  /* USER CODE BEGIN ETH_Init 1 */
 
  /* USER CODE END ETH_Init 1 */
  heth.Instance = ETH;
  MACAddr[0] = 0x00;
  MACAddr[1] = 0x80;
  MACAddr[2] = 0xE1;
  MACAddr[3] = 0x00;
  MACAddr[4] = 0x00;
  MACAddr[5] = 0x00;
  heth.Init.MACAddr = &MACAddr[0];
  heth.Init.MediaInterface = HAL_ETH_RMII_MODE;
  heth.Init.TxDesc = DMATxDscrTab;
  heth.Init.RxDesc = DMARxDscrTab;
  heth.Init.RxBuffLen = 1524;
 
  /* USER CODE BEGIN MACADDRESS */
 
  /* USER CODE END MACADDRESS */
 
  if (HAL_ETH_Init(&heth) != HAL_OK)
  {
    Error_Handler();
  }
 
  memset(&TxConfig, 0 , sizeof(ETH_TxPacketConfig));
  TxConfig.Attributes = ETH_TX_PACKETS_FEATURES_CSUM | ETH_TX_PACKETS_FEATURES_CRCPAD;
  TxConfig.ChecksumCtrl = ETH_CHECKSUM_IPHDR_PAYLOAD_INSERT_PHDR_CALC;
  TxConfig.CRCPadCtrl = ETH_CRC_PAD_INSERT;
  /* USER CODE BEGIN ETH_Init 2 */
 
  	HAL_ETH_MspInit(&heth);
    HAL_ETH_Start_IT(&heth);
    HAL_ETH_IRQHandler(&heth);
 
 
  /* USER CODE END ETH_Init 2 */
 
}
 
/**
  * @brief GPIO Initialization Function
  * @param None
  * @retval None
  */
static void MX_GPIO_Init(void)
{
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */
 
  /* GPIO Ports Clock Enable */
  __HAL_RCC_GPIOC_CLK_ENABLE();
  __HAL_RCC_GPIOA_CLK_ENABLE();
  __HAL_RCC_GPIOB_CLK_ENABLE();
  __HAL_RCC_GPIOG_CLK_ENABLE();
 
/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}
 
/* USER CODE BEGIN 4 */
void HAL_ETH_RxCpltCallback(ETH_HandleTypeDef *heth)
{
 
	flag = 1;
}
/* USER CODE END 4 */
 
/* MPU Configuration */
 
void MPU_Config(void)
{
  MPU_Region_InitTypeDef MPU_InitStruct = {0};
 
  /* Disables the MPU */
  HAL_MPU_Disable();
 
  /** Initializes and configures the Region and the memory to be protected
  */
  MPU_InitStruct.Enable = MPU_REGION_ENABLE;
  MPU_InitStruct.Number = MPU_REGION_NUMBER0;
  MPU_InitStruct.BaseAddress = 0x0;
  MPU_InitStruct.Size = MPU_REGION_SIZE_4GB;
  MPU_InitStruct.SubRegionDisable = 0x87;
  MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
  MPU_InitStruct.AccessPermission = MPU_REGION_NO_ACCESS;
  MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;
  MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE;
  MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;
  MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
 
  HAL_MPU_ConfigRegion(&MPU_InitStruct);
  /* Enables the MPU */
  HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);
 
}
 
/**
  * @brief  This function is executed in case of error occurrence.
  * @retval None
  */
void Error_Handler(void)
{
  /* USER CODE BEGIN Error_Handler_Debug */
  /* User can add his own implementation to report the HAL error return state */
  __disable_irq();
  while (1)
  {
  }
  /* USER CODE END Error_Handler_Debug */
}
 
#ifdef  USE_FULL_ASSERT
/**
  * @brief  Reports the name of the source file and the source line number
  *         where the assert_param error has occurred.
  * @param  file: pointer to the source file name
  * @param  line: assert_param error line source number
  * @retval None
  */
void assert_failed(uint8_t *file, uint32_t line)
{
  /* USER CODE BEGIN 6 */
  /* User can add his own implementation to report the file name and line number,
     ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
  /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

11 REPLIES 11
Pavel A.
Evangelist III

Why is HAL_ETH_MspInit called in line 243 after Init in line 232?

Why is HAL_ETH_IRQHandler called in line 245?

Have you tried to deal with any interrupt before?

MHens.2
Associate II

Side note: Are you sure about the MAC address? all 00-00-00 after the OUI seems unlikely.

I tried to do the order of function calls as in the documentation for the driver.

Removed HAL_UART_IRQHandler. I experimented

/*
The ETH HAL driver can be used as follows:
 
      (#)Declare a ETH_HandleTypeDef handle structure, for example:
         ETH_HandleTypeDef  heth;
 
      (#)Fill parameters of Init structure in heth handle
 
      (#)Call HAL_ETH_Init() API to initialize the Ethernet peripheral (MAC, DMA, ...)
 
      (#)Initialize the ETH low level resources through the HAL_ETH_MspInit() API:
          (##) Enable the Ethernet interface clock using
                (+++)  __HAL_RCC_ETH1MAC_CLK_ENABLE()
                (+++)  __HAL_RCC_ETH1TX_CLK_ENABLE()
                (+++)  __HAL_RCC_ETH1RX_CLK_ENABLE()
 
          (##) Initialize the related GPIO clocks
          (##) Configure Ethernet pinout
          (##) Configure Ethernet NVIC interrupt (in Interrupt mode)
 
      (#) Ethernet data reception is asynchronous, so call the following API
          to start the listening mode:
          (##) HAL_ETH_Start():
               This API starts the MAC and DMA transmission and reception process,
               without enabling end of transfer interrupts, in this mode user
               has to poll for data reception by calling HAL_ETH_ReadData()
          (##) HAL_ETH_Start_IT():
               This API starts the MAC and DMA transmission and reception process,
               end of transfer interrupts are enabled in this mode,
               HAL_ETH_RxCpltCallback() will be executed when an Ethernet packet is received
 
      (#) When data is received user can call the following API to get received data:
          (##) HAL_ETH_ReadData(): Read a received packet
*/

This is the default configuration.

Ethernet transfer with this MAC is successful

> Removed HAL_UART_IRQHandler.

But is there an ETH interrupt handler in your code and does it call HAL_UART_IRQHandler ?

And where do you call send?

There is an interrupt handler.

In the debugger, I saw that it goes into it once and the HAL_ETH_ERROR_DMA error is processed

I don't know what's wrong and how to fix it

DMACSR signals 0x00004080 (receive buffer unavailable) 

Pavel A.
Evangelist III

> DMACSR signals 0x00004080 (receive buffer unavailable) 

Where the buffers and descriptors are set up?

Please take an existing working example first and learn how it works.

I use H743. I didn't configure DMA myself. As I understand it, the Ethernet MAC has its own DMA and it is configured in the functions: HAL_ETH_Init, HAL_ETH_Start_IT

Should I have taken any additional steps?

Where can I see a suitable example? (with up-to-date drivers and without LWIP)