cancel
Showing results for 
Search instead for 
Did you mean: 

Bug STM32F427VGT6 SDIO 4bit mode doesn't work

vekli
Associate II

STM32Cube FW_F4 V1.28

STM32CubeMX 6.11.1

file main.c line 209 function static void MX_SDIO_SD_Init(void)

hsd.Init.BusWide = SDIO_BUS_WIDE_4B;

fix

 hsd.Init.BusWide = SDIO_BUS_WIDE_1B;

Related post.

https://community.st.com/t5/stm32cubemx-mcus/sdio-interface-not-working-in-4bits-with-stm32f4-firmware/td-p/591776

1 ACCEPTED SOLUTION

Accepted Solutions

No need to report it as it was already treated in https://community.st.com/t5/stm32cubemx-mcus/sdio-interface-not-working-in-4bits-with-stm32f4-firmware/m-p/591803#M26033 . and the internal ticket number 155983 was opened.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
mƎALLEm
ST Employee

Hello,

Your comment is not clear. Do you mean that the solution proposed solution in https://community.st.com/t5/stm32cubemx-mcus/sdio-interface-not-working-in-4bits-with-stm32f4-firmware/td-p/591776 doesn't work?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Hi SofLit. I just reported bug for setup above and it can be fixed as proposed in post.

No need to report it as it was already treated in https://community.st.com/t5/stm32cubemx-mcus/sdio-interface-not-working-in-4bits-with-stm32f4-firmware/m-p/591803#M26033 . and the internal ticket number 155983 was opened.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.