cancel
Showing results for 
Search instead for 
Did you mean: 

Are there a ethernet shield to STM32F303ZE?

Geraldo Pereira
Associate II

Hi Guys,

I´ve bought the STM32F303ZE Nucleo-144 kit. Are there a ethernet shield to this kit? If so, where can I read and buy about?

A Shiled like this to other kit of st:

https://www.carminenoviello.com/2015/08/28/adding-ethernet-connectivity-stm32-nucleo/

Thanks,

Geraldo Pereira.

7 REPLIES 7
Geraldo Pereira
Associate II

I´ve just read this kit doesn´t support ethernet.

The F3 doesn't have an ethernet controller, but this wouldn't preclude using a shield with a Wiz or Microchip Ethernet via SPI

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Uwe Bonnes
Principal III

Consider using a Nucleo144 with Ethernet.

Geraldo Pereira
Associate II

Hi Bonnes and Clive1,

Thanks. After this post, I´ve searched (link https://www.st.com/en/evaluation-tools/stm32-nucleo-boards.html) and see other kits that have ethernet support. I think with the kit NUCLEO-H743ZI2 (STM32H743ZIT6U) I´ll be able to construct a prototype to send UDP message, like socket in c, over internet.

Do you have a hint to me? I need a kit to read the three phase voltage anc current of a grid and send the arrays (of variable length) to a remote PC using some protocol like c socket. I´ll be greatefull about any hint.

Best regards,

Geraldo.

Thanks Clive1,

What shileld or Microchip ethernet do you suggest to me? I´m new with this boards and any hints will be great.

Thanks,

Geraldo.

Uwe Bonnes
Principal III

Reconsider the H7. H7 is much more complex. F7 or even F4 might be ennough. If you need good ADC behaviour, read also the Application notes regarding ADC and F2/4/7/H7. Special considerations may be needed for good resolution.