cancel
Showing results for 
Search instead for 
Did you mean: 

AN2606 ST Bootloader using FDCan with STM32H563 -> Bug in GPIOx or FDCANx Mapping?

jherrmann1
Associate II

Hello all,

I would like to use the ST Bootloader which is described in the Application Note AN2606.

https://www.st.com/resource/en/application_note/an2606-stm32-microcontroller-system-memory-boot-mode-stmicroelectronics.pdf.

The used controller is the STM32H563. Under point 50.1 it is described that FDCAN1 must be used. As FDCAN1_Rx pin PB5 and FDCAN1_Tx pin PB13 is defined. But these two GPIOs go to FDCAN2 and not to FDCAN1.

AN2606_STM32H563_FDCAN_Problem.png

Can you help me further on this, which pins or which FDCANx should be used?

Thanks in advance!

Jannik

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Guru

The correct FDCAN and pins are:

  • FDCAN2_RX : PB5
  • FDCAN2_TX : PB13

https://community.st.com/t5/stm32-mcus-products/stm32h5-need-bootloader-pins/td-p/595584

 

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

3 REPLIES 3
TDK
Guru

The correct FDCAN and pins are:

  • FDCAN2_RX : PB5
  • FDCAN2_TX : PB13

https://community.st.com/t5/stm32-mcus-products/stm32h5-need-bootloader-pins/td-p/595584

 

If you feel a post has answered your question, please click "Accept as Solution".
KDJEM.1
ST Employee

Hello @jherrmann1 and welcome to the Community :),

This is already reported here.

For FDCAN bootloader, you should use FDCAN2 with correct pins are : 
FDCAN2_RX : PB5
FDCAN2_TX : PB13

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

jherrmann1
Associate II

thank you for the quick reply, that helped me a lot!