2025-01-14
10:11 PM
- last edited on
2025-01-14
11:44 PM
by
Maxime_MARCHETT
Hello,
I'm interested in Power Line Communication and the X-NUCLEO-PLM01A1.
I would like to confirm before purchasing.
What is the role of the PLM connector (CN1)?
Is it a PLC line?
If so, is the Lab DC Supply Inout Connector (CN2) just a power supply?
The PLM Connector appears to be a Power Amplifier Output. Does this Connector use a PLC Line?
To connect two or more boards, you need to connect the PLM Connector (CN1) to each other.
What is the role of CN1?
Will it be a problem if I don't connect the CN1s to each other?
*This post has been translated from Korean to comply with the ST Community guidelines.
2025-01-15 01:16 AM
See the User Manual: it's where you make the PLM connection - it is the comms link between the two boards:
via: https://www.st.com/en/ecosystems/x-nucleo-plm01a1.html#documentation
See also the documentation for the ST7580 chip:
https://www.st.com/en/interfaces-and-transceivers/st7580.html