2025-02-14 5:55 AM - last edited on 2025-12-29 10:02 AM by ELABI.1
Hi, im planing on running computer vision DL models on multiple STM32 boards. At this moment I will compare a STM32MP256F-EV1 with a STM32H747-DISCO, however i only bought the B-CAMS-OMV and is not the same connector on the MP board. IS there any way o run this camera module on both board, can I just get an adapter from the 30-pin ZIF to the CSI connector?Also i dont is the any suplementary information about the ZIF connector
2025-10-10 8:24 PM
hi
an I just get an adapter from the 30-pin ZIF to the CSI connector?
----you can't do this, for this camera is using RGB signals, the CSI connector is using the mipi-csi signals.