2022-05-11 06:01 AM
Hello,
I have found out that connection from transceiver pins CAN_RX and CAN_TX are connected to CAN_TX and CAN_RX.
I mean :
from CAN transceiver to stm32f105
CAN_RX -----------------------------> CAN_TX
CAN_TX------------------------------> CAN_RX
Is there anyway to fix the issue in software?
Thank you.
Solved! Go to Solution.
2022-05-12 01:26 AM
>Is there anyway to fix the issue in software?
If you really really reeeeeally need to, you could develop your own softCANBUS, that said i wouldnt like to be you.
The Easier choice is to modify the hardware and run the production again.
2022-05-11 01:39 PM
No.
JW
2022-05-12 01:26 AM
>Is there anyway to fix the issue in software?
If you really really reeeeeally need to, you could develop your own softCANBUS, that said i wouldnt like to be you.
The Easier choice is to modify the hardware and run the production again.
2022-05-12 01:28 AM
Ja, the easier way is to modify the hardware.
Thanks
2022-05-12 01:28 AM
Thank you @Community member