cancel
Showing results for 
Search instead for 
Did you mean: 

Wrong pins for CAN_RX and CAN_TX

NASI
Senior

Hello,

I have found out that connection from transceiver pins CAN_RX and CAN_TX are connected to CAN_TX and CAN_RX.

I mean :

from CAN transceiver to stm32f105

CAN_RX -----------------------------> CAN_TX

CAN_TX------------------------------> CAN_RX

Is there anyway to fix the issue in software?

Thank you.

1 ACCEPTED SOLUTION

Accepted Solutions
Javier1
Principal

>Is there anyway to fix the issue in software?

If you really really reeeeeally need to, you could develop your own softCANBUS, that said i wouldnt like to be you.

The Easier choice is to modify the hardware and run the production again.

we dont need to firmware by ourselves, lets talk

View solution in original post

4 REPLIES 4

No.

JW

Javier1
Principal

>Is there anyway to fix the issue in software?

If you really really reeeeeally need to, you could develop your own softCANBUS, that said i wouldnt like to be you.

The Easier choice is to modify the hardware and run the production again.

we dont need to firmware by ourselves, lets talk
NASI
Senior

Ja, the easier way is to modify the hardware.

Thanks

Thank you @Community member​