2017-04-12 3:03 AM
Hi,
we are using the CLI of the st-link utility to flash some STM32-controller in the production. Now I had to install a newer version (CLI v2.0.0 vs. CLI v3.0.0) to support the STM32F413.
With this new version the behavior of the -Run command changed. In v2.0.0 the -Run command will automatically start the application after programming. In v3.0.0 it leads to a prompt 'run application to exit', which has to be confirmed by pressing ENTER.
Before the -Run command was useful to automate manual steps, now it adds another. Is there a way to skip the prompt?
#st-link-utility2017-04-13 1:53 AM
Hi
W_hle.Stefan
,We are aware of this
behavior, but th
ere is no way
to skip the
'run application to exit'
promptwith theCLI v3.0.0
This
behavior
will be fixed in the nextversion.We apologize for any inconvenience this may have caused you.
Thanks
Imen
2017-07-10 6:42 AM
Any news on when V3.1.0 will be there? I've got the same problem. I'm not able to use the CLI for automating the process now.
2017-07-10 9:23 AM
Hello
pbaan93
,I would inform you that a new release will be available soon
to fix this issue.
With Regards
Imen
2017-08-03 8:40 AM
Hello, Has it been released?
We have issues with CLI command on STM32L479 512 Kb with SWD, seems few bugs.
- whenever we touch the option byte, the dual bank is selected, it is impossible to select single bank
- as soon as the read out protection is set to 1 the memory returns to dual bank, then the upper 256K bank is erased
- it is impossible to run the application with the Run command, CLI returns no target connected
- the '-Rst' command has no effect.
Please let me know we need a fix very urgently.
Thanks for your help.
B.Rgds/F
2017-08-03 9:06 AM
STM32l476, not STML479 sorry.
Thanks/F
2017-08-04 2:50 AM
As a temporary workaround you can use a VBScript (a text file with *.vbs extension) to send the Enter key, I'm currently not on a Windows machine to try, but something like this should work:
Set WshShell = WScript.CreateObject('WScript.Shell')
WshShell.Run('D:\Utils\st-link.exe -foo -bar', 9)WScript.Sleep 5000WshShell.SendKeys '{ENTER}'MSDN Links:
https://msdn.microsoft.com/en-us/library/d5fk67ky(v=vs.84).aspx
,https://msdn.microsoft.com/en-us/library/6t81adfd(v=vs.84).aspx
,https://msdn.microsoft.com/en-us/library/8c6yea83(v=vs.84).aspx
2017-08-04 4:23 AM
Dear Florent,
You need to contact your local FAE , we may prepare a patch for your customer if really urgent.
How things are going in your location?, very long time not seeing you ..exactly 10 years ago. { See my profile }
Cheers
STOne -32
2018-08-03 1:41 AM
-NoPrompt is the solution
Great work!