2021-05-19 10:14 PM
Facing some problems related to emulation circuit in STM32MP157C-DK2. STM32F103CBT6 micro-controller used in this application requires firmware i.e. STLinkv2/1. Please provide the hex file for firmware-STLinkv2/1 and necessary details to program the blank chip (STM32F103CBT6) and use it for STM32MP157C.
2021-05-20 12:03 AM
ST does not provide publicly the STLink firmware.
JW
2021-05-20 12:48 AM
Can you tell how to get firmware for STLinkV2/1 or STM32F103CBT6 chip with preloaded firmware for STLinkV2/1?
2021-05-20 6:06 AM
The firmware is already preloaded into the STM32F103CBT6 if you own a ready-made STM32MP157C-DK2. You can then directly connect the ST-LINK/V2-1 to your computer and update the firmware using e.g. STM32CubeProgrammer. Use a direct USB connection, i.e. without USB hub inbetween, if you encounter connection issues.
Regards
/Peter
2021-05-20 6:19 AM
At a module level ST offers the ST-LINK/V3MODS
https://www.st.com/en/development-tools/stlink-v3mods.html
2021-05-20 6:49 AM
The bootloader and firmware files float around in the internet.
2021-05-20 10:19 PM
Actually we are making a custom PCB board based on STM32MP157C-DK2. So for that we require STlink-v2.1 firmware hex files to flash the blank chip (STM32F103CBT6).
2021-05-20 10:22 PM
Okay, but we are unable to find any. Can you provide the link for STLink-v2.1 firmware hex file (not StLinkv2)?
2021-05-21 12:47 AM
The ST-LINK/V2-1 acts as debugger/programmer and is normally not required for an end application with the STM32MP157C. The firmware of the ST-LINK may only be used for original development kits from ST. As already mentioned by @Community member STMicroelectronics provides an ST-LINK/V3MODS if you want to include it in your board.
BTW: please read the Terms of Use and the Open Reference Material License Agreement, which can be found at the website of the STM32MP157C-DK2.
Regards
/Peter