Skip to main content
STehA.1
Associate II
February 1, 2024
Question

How to program clone ST-Link V2.1

  • February 1, 2024
  • 2 replies
  • 4491 views

Hi,

 

I am making my clone ST-Link v2.1 device using 128 KB STM32F103CBT6 mcu. Please help clarify as follows:

 

1) Do I need to set Boot 0 pin = 1 and Boot 1 pin = 0 in order to program the bootloader into the device?

2) Do I need to set Boot 0 pin = 0 and Boot 1 pin = 0 (don't care) in order to program the st-link v2.1 firmware into the device?

3) Where/How can I download the bootloader and the stlink v2.1 firmware from ST?

Help much appreciated.

SAM

    This topic has been closed for replies.

    2 replies

    AScha.3
    Super User
    February 1, 2024

    1 + 2 : depends on : how you want to flash the F103 ? in bootloader mode or with st-link (or j-link , dap...)

    3 . STM has no "free" or open source st-link firmware ; its only on the st-link adapters, you can buy from STM (or distributor ). So NO download with bootloader or stlink v2.1 firmware from STM .

     

    But you can make another debug probe : cmsis DAP , Black Magic Probe

    https://github.com/RadioOperator/STM32F103C8T6_CMSIS-DAP_SWO/tree/master

    https://mcuoneclipse.com/2019/06/23/black-magic-open-source-debug-probe-for-arm-with-eclipse-and-gdb/

     

    --- or search on github for st-link , you can find some clones there.

    If you feel a post has answered your question, please click on " Best Answer ".
    STehA.1
    STehA.1Author
    Associate II
    February 1, 2024

    Hi Asha,

     

    Thank you for the reply. I have clone ST-Link v2 or ST-Link v2.1 (pendrive shape) that I am thinking about using it to program the bootloader and the ST-Link firmware into my going to be clone ST-Link v2.1 (I wish). Later, I will download the STM32 Cube Programmer for the purpose. The clone ST-Link comes with SWDIO, SWCLK, GND and 3V3 pins.

    Any helps from you are much appreciated. Thank you.

     

    SAM