2019-03-12 7:39 AM
I see reference to the jumper between D2 and GND, but I don't see any explanation regarding it's use and when it should be on or when it should be off. I'd like an explanation of this jumper please.
Solved! Go to Solution.
2019-03-12 12:35 PM
OK, I get it...as mentioned above, it's something that was shipped with the board and essentially is just changing the frequiency of the green led blink...
Closing this post.
2019-03-12 7:41 AM
I'm sorry, I have a NUCLEO_L432KC board with the jumper between pins D2 and GND that I'm inquiring about.
Thanks.
2019-03-12 8:17 AM
My GUESS is that the pre-loaded the demo firmware looks at this pin to decide what to do. Or else this is an unused pin in the demo firmware and ST wanted to ship an spare jumper clip with the board and that was the safest place to put it :) You ought to be able to get the source for the pre-loaded demo code from (I don't remember where) and find out, if you care.
2019-03-12 9:44 AM
Hi @JB.5lacker ,
Referring to UM1956, in the section "5.1 Getting started", we have the following:
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2019-03-12 12:35 PM
OK, I get it...as mentioned above, it's something that was shipped with the board and essentially is just changing the frequiency of the green led blink...
Closing this post.