cancel
Showing results for 
Search instead for 
Did you mean: 

WB55RG/WB15CC and PLC01A1

TLans.1
Associate II

Is NUCLEO-WB55RG/WB15CC compatible with X-NUCLEO-PLC01A1?

I want to develop a controller that supports BLE and thought of starting with a combination of these two boards. Would be helpful if someone can confirm that these boards are compatible and can be stacked and work together.

Thanks. 

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @TLans.1 

As we can see on the UM1918, the X-NUCLEO-PLC01A1 can be Plugged onto any STM32 Nucleo board through the Arduino UNO R3 connectors. So, the Shield is Compatible with the NUCLEO-WB55RG/WB15CC that includes the Arduino R3 Connectors.

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
STTwo-32
ST Employee

Hello @TLans.1 

As we can see on the UM1918, the X-NUCLEO-PLC01A1 can be Plugged onto any STM32 Nucleo board through the Arduino UNO R3 connectors. So, the Shield is Compatible with the NUCLEO-WB55RG/WB15CC that includes the Arduino R3 Connectors.

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.