2024-07-17 3:34 AM - last edited on 2024-08-05 6:27 AM by Amel NASRI
Is NUCLEO-WB55RG/WB15CC compatible with X-NUCLEO-PLC01A1?
I want to develop a controller that supports BLE and thought of starting with a combination of these two boards. Would be helpful if someone can confirm that these boards are compatible and can be stacked and work together.
Thanks.
Solved! Go to Solution.
2024-08-13 1:42 AM
Hello @TLans.1
As we can see on the UM1918, the X-NUCLEO-PLC01A1 can be Plugged onto any STM32 Nucleo board through the Arduino UNO R3 connectors. So, the Shield is Compatible with the NUCLEO-WB55RG/WB15CC that includes the Arduino R3 Connectors.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-08-13 1:42 AM
Hello @TLans.1
As we can see on the UM1918, the X-NUCLEO-PLC01A1 can be Plugged onto any STM32 Nucleo board through the Arduino UNO R3 connectors. So, the Shield is Compatible with the NUCLEO-WB55RG/WB15CC that includes the Arduino R3 Connectors.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.