cancel
Showing results for 
Search instead for 
Did you mean: 

USART6 in STM32F429ZI (nucleo)

PanMaltan
Associate

Hello All,

 

its my first post here - i just started my journey with Nucleo 429ZI board.

I wrote simple app where i want to receive i different way(with-and-without interrupt) data from USART2 and USART6 ports.

 

While i dont have any troubles getting data on USART2 RX pin, i can't get antyhing on USART6 RX pin (im using same output terminal for both)

Hereby config (i done everything by clicking in IOC configurator):

for USART2 and USART6 - autogenerated code

 

 if(huart->Instance==USART2)
  {
  /* USER CODE BEGIN USART2_MspInit 0 */

  /* USER CODE END USART2_MspInit 0 */
    /* Peripheral clock enable */
    __HAL_RCC_USART2_CLK_ENABLE();

    __HAL_RCC_GPIOA_CLK_ENABLE();
    __HAL_RCC_GPIOD_CLK_ENABLE();
    /**USART2 GPIO Configuration
    PA3     ------> USART2_RX
    PD5     ------> USART2_TX
    */
    GPIO_InitStruct.Pin = GPIO_PIN_3;
    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
    GPIO_InitStruct.Alternate = GPIO_AF7_USART2;
    HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

    GPIO_InitStruct.Pin = GPIO_PIN_5;
    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
    GPIO_InitStruct.Alternate = GPIO_AF7_USART2;
    HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);

  /* USER CODE BEGIN USART2_MspInit 1 */

  /* USER CODE END USART2_MspInit 1 */
  }
 else if(huart->Instance==USART6)
  {
  /* USER CODE BEGIN USART6_MspInit 0 */

  /* USER CODE END USART6_MspInit 0 */
    /* Peripheral clock enable */
    __HAL_RCC_USART6_CLK_ENABLE();

    __HAL_RCC_GPIOC_CLK_ENABLE();
    /**USART6 GPIO Configuration
    PC6     ------> USART6_TX
    PC7     ------> USART6_RX
    */
    GPIO_InitStruct.Pin = GPIO_PIN_6|GPIO_PIN_7;
    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
    GPIO_InitStruct.Alternate = GPIO_AF8_USART6;
    HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

  /* USER CODE BEGIN USART6_MspInit 1 */

  /* USER CODE END USART6_MspInit 1 */
  }

 

 

Pins for USART6 are PC6 and PC7

Pins for USART2 are PA3 and PD5

 

code in main is very simple:

 

 

 while (1)
  {
    /* USER CODE END WHILE */

    /* USER CODE BEGIN 3 */

	  //ret = HAL_UART_Transmit(&huart2, utx_buff, 12, 1000);
	  HAL_GPIO_TogglePin(LD1_GPIO_Port,LD1_Pin);
	  HAL_Delay(1000);
	  HAL_UART_Receive(&huart2, temp, 5, 1000);
	  HAL_Delay(1000);
	  HAL_UART_Receive(&huart6, temp2, 5, 1000);
}
where:
uint8_t temp[8];
uint8_t temp2[8];

 

im observing temp and temp2 arrays in 'live' view in STM IDE.

While temp is filled with data when i send data over terminal, i cannot see any change in temp2.

 

Thanks for all support!

3 REPLIES 3
Pavel A.
Evangelist III

On Nucleo boards some pins are soldered to something and cannot be used freely. Please check the pin assignment in the documentation. If PC6 and PC7 are not available, try to find alternatives for USART6 (CubeMX/IDE will show) or use other UART.

 

SofLit
ST Employee

And if you swap the position call of : HAL_UART_Receive(&huart6 ...); and HAL_UART_Receive(&huart2 ...);

	  HAL_GPIO_TogglePin(LD1_GPIO_Port,LD1_Pin);
	  HAL_Delay(1000);
	  HAL_UART_Receive(&huart6, temp2, 5, 1000);
	  HAL_Delay(1000);
	  HAL_UART_Receive(&huart2, temp, 5, 1000);

 Meanwhile, I suggest to use DMA or interrupt for Rx instead of that kind of programming.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: This is NOT an online support (https://ols.st.com) but a collaborative space. So please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.

What hardware do you use to transmit data from PC to the UARTs? An USB-UART converter, or something else?

JW