cancel
Showing results for 
Search instead for 
Did you mean: 

Unsufficient disk space on current disk

alpaltunsoy
Associate II

Hello everyone, i am currently working on STM32 NUCLEO-L073RZ Projects with Ardunio Ide. I did not change anything from yesterday only i install mbed studio and after installation i delete. I did not do anything with mbed just installation,  and i took these errors attached with pictures. There are also Fail.txt file in Disk. How can i solve problems. All jumpers are located in correct place.

 

Sketch uses 8024 bytes (4%) of program storage space. Maximum is 196608 bytes.
Global variables use 868 bytes (4%) of dynamic memory, leaving 19612 bytes for local variables. Maximum is 20480 bytes.
"C:\Users\alpal\AppData\Local\Arduino15\packages\STM32\tools\STM32Tools\1.4.0/tools/win/massStorageCopy.bat" -I "C:\Users\alpal\AppData\Local\Temp\arduino\sketches\03AC7BC7F6E3ABB77F4268DAA235E17A/sketch_may14a.ino.bin" -O "NODE_L073RZ"

Insufficient disk space on current disk.
Insert another disk and type <Return> to continue...

Insufficient disk space on current disk.
Insert another disk and type <Return> to continue... Failed uploading: uploading error: exit status 2Ekran görüntüsü 2024-05-14 190908.png

 

 

14 REPLIES 14

WhatsApp Image 2024-05-14 at 19.31.53.jpeg

 

Everything is located in correct way and it didnt work. i supply 3.3v from another voltage source it does not work

Actually my code was working and after 1 day with closed it doesnt

Not sure I'd power it this way.

Can you connect to it if self-powered?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Yes and nothing changed

Error suggests the L073 isn't functional/viable, so could be damaged.

Disconnect external supplies, check 5V, 3.3V and VIN voltages at the headers.

Check 5V and U5V jumper, which is selecting the USB 5V as primary supply

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..