2020-06-27 4:06 PM
Hi,
I'm trying to program my 32L0538DISCOVERY board using the STM32CubeIDE but after trying to upload to it it says that:
and offers me to update the st link firmware with st link upgrade so it fin'd it there and everything but when I hit the "Open in update mode" it seems to disconnect the usb port and nothing happens afterwards...
Any idea how to fix that?
2020-06-27 4:21 PM
Also can't Upgrade my ST link V2 programmer saying it doesn't find it but it does appear under device manager under USB (But not COM port)
2020-06-30 8:08 AM
Un-plug and re-plug the board as indicated in the screenshot above. This is required on some boards, on some boards it is enough to just click open in update mode.
2020-07-09 12:04 PM
Apperantly that's a driver issue...
2020-07-12 3:21 AM
Yeah so apperantly nothing makes it work and when opening in update mode is simply disconnect the port and shows as error.