2020-07-11 10:37 AM
Hello,
Wondering if anyone out there is knowledgeable in the ST-LINK V3 Bridge API? I'm working on a personal project developing a GUI application that uses the API to provide something like a Bus Pirate type development tool. If you want to look at bad C/C++ code the project is on GitHub. I've gotten the GPIO portion to work and am working on I2C. My specific question is this:
The I2C read/write methods take a parameter for returning the actual number of bytes written on the bus. Here's one of the methods signature:
Brg_StatusT WriteI2C(const uint8_t *pBuffer, uint16_t Addr, uint16_t SizeInBytes, uint16_t *pSizeWritten);pSizeWritten is the parameter in question. It seems to always return zero even though the BrgStatusT return value is BRG_NO_ERR. I've looked at the bus on the scope and can see bytes written/read and they appear correct.
So is this a misuse/misunderstanding of the API on my part or a bug in the bridge sources or a bug in the DLL or cosmic interference??
EDIT: Forgot any kind of version info:
ST-LINK V3SET - fw ver V3J7M2B4S1
ST-LINK V3 Bridge API version - 1
ST-LINK USB Driver DLL version (from windows) - 5.1.3.0, this I think corresponds to 2.36.26 of STSW-LINK007
WIN 10 machine
Thanks for your time,
Andy
Solved! Go to Solution.
2020-07-11 11:31 AM
So it appears I found my own answer. I read the sources several times but missed a little tidbit:
/**
* @ingroup I2C
* @brief This routine allows to transmit bytes on the I2C interface, in the mode initialized by Brg::InitI2C().\n
* In master mode I2C the size bytes are transmitted in one I2C transaction ((re)start- addr- data -stop)
* even if data may be split into several USB packets.
* @param[in] Addr I2C slave address used in master mode (default 7bit):
* use #I2C_10B_ADDR(Addr) if it is a 10bit address.
* @param[in] pBuffer Pointer on data buffer with data to be read.
* @param[in] SizeInBytes Data size to be read in bytes (min 1, max data buffer size).
* @param[out] pSizeWritten If not NULL and in case of error, pSizeWritten returns the number of bytes
* transmitted before the error.
*
* @retval #BRG_NO_STLINK If Brg::OpenStlink() not called before
* @retval #BRG_COM_INIT_NOT_DONE If I2C is not initialized
* @retval #BRG_I2C_ERR In case of I2C error
* @retval #BRG_COM_CMD_ORDER_ERR If low level I2C function call order is not consitent (Start, Cont, Stop)
* @retval #BRG_NO_ERR If no error
*/pSizeWritten is only filled with a value in the case of an error. So I suppose with no error its safe to assume SizeWritten == SizeInBytes.
2020-07-11 11:31 AM
So it appears I found my own answer. I read the sources several times but missed a little tidbit:
/**
* @ingroup I2C
* @brief This routine allows to transmit bytes on the I2C interface, in the mode initialized by Brg::InitI2C().\n
* In master mode I2C the size bytes are transmitted in one I2C transaction ((re)start- addr- data -stop)
* even if data may be split into several USB packets.
* @param[in] Addr I2C slave address used in master mode (default 7bit):
* use #I2C_10B_ADDR(Addr) if it is a 10bit address.
* @param[in] pBuffer Pointer on data buffer with data to be read.
* @param[in] SizeInBytes Data size to be read in bytes (min 1, max data buffer size).
* @param[out] pSizeWritten If not NULL and in case of error, pSizeWritten returns the number of bytes
* transmitted before the error.
*
* @retval #BRG_NO_STLINK If Brg::OpenStlink() not called before
* @retval #BRG_COM_INIT_NOT_DONE If I2C is not initialized
* @retval #BRG_I2C_ERR In case of I2C error
* @retval #BRG_COM_CMD_ORDER_ERR If low level I2C function call order is not consitent (Start, Cont, Stop)
* @retval #BRG_NO_ERR If no error
*/pSizeWritten is only filled with a value in the case of an error. So I suppose with no error its safe to assume SizeWritten == SizeInBytes.