2023-02-08 1:41 AM
I've have a custom board with a STM32G031,from the board we have access to the following MCU pins:
I've connected this 4 pins to a ST-LINK/V2. Like this (left) mcu, (right) st-link.
The current delivered by PSU goes to almost 0 after trying to flash (around 0.004A from the correct 0.041A). When trying to flash the uC these are the errors/log I get:
10:37:32 : ST-LINK SN : 55FF6E067871515343241267
10:37:32 : ST-LINK FW : V2J39S7
10:37:32 : Board : --
10:37:32 : Voltage : 2,60V
10:37:32 : SWD freq : 4000 KHz
10:37:32 : Connect mode: Normal
10:37:32 : Reset mode : Software reset
10:37:32 : Device ID : 0x466
10:37:32 : Revision ID : Rev 1.1
10:37:35 : Error: Database: There's no active configuration for this device. All the 6 configurations are disabled!
10:37:35 : Debug in Low Power mode is not supported for this device.
10:37:36 : UPLOADING OPTION BYTES DATA ...
10:37:36 : Bank : 0x00
10:37:36 : Address : 0x40022020
10:37:36 : Size : 108 Bytes
10:37:36 : Error: Uploading Option Bytes bank: 0 failed
10:37:38 : Error: Initializing the Option Bytes failed
10:37:38 : Disconnected from device.
Isolating the errors:
Error: Database: There's no active configuration for this device. All the 6 configurations are disabled!
Error: Uploading Option Bytes bank: 0 failed
Error: Initializing the Option Bytes failed
Any ideas on how to solve this?
Thanks!
Solved! Go to Solution.
2023-02-08 6:00 AM
Your pin list omit GND i hope connected
2023-02-08 3:10 AM
Im using stm32g030j6Mx without selecting SW pins and i dont have this issue
Check all posibilities.
2023-02-08 3:34 AM
Hi Javier,
I'm using STM32G031J6M6 & CubeProgrammer v2.11.0.
I've tried right now other modes. Normal is the one of my post, hotplug has the same errors but the current doesn't change, under reset same errors & also current drop to almost 0, finally power down doesn't react at all "No STM32 target found!" at all times.
This is the ST-LINK configuration I've been using until now:
2023-02-08 3:50 AM
Disconect power from your board
connect stlink start in power down mode
click connect
plug power to board
2023-02-08 5:01 AM
> 10:37:35 : Error: Database: There's no active configuration for this device. All the 6 configurations are disabled!
looks like your ST-LINK may need a firmware update?
hth
KnarfB
2023-02-08 5:40 AM
I updated the ST-LINK but same problem:
14:40:07 : ST-LINK SN : 55FF6E067871515343241267
14:40:07 : ST-LINK FW : V2J39S7
14:40:07 : Board : --
14:40:07 : Voltage : 2,60V
14:40:07 : SWD freq : 4000 KHz
14:40:07 : Connect mode: Normal
14:40:07 : Reset mode : Software reset
14:40:07 : Device ID : 0x466
14:40:07 : Revision ID : Rev 1.1
14:40:10 : Error: Database: There's no active configuration for this device. All the 6 configurations are disabled!
14:40:11 : UPLOADING OPTION BYTES DATA ...
14:40:11 : Bank : 0x00
14:40:11 : Address : 0x40022020
14:40:11 : Size : 108 Bytes
14:40:11 : Error: Uploading Option Bytes bank: 0 failed
14:40:11 : Error: Initializing the Option Bytes failed
14:40:11 : Disconnected from device.
2023-02-08 5:41 AM
Can you please expand on that? If I tri to connect with the board disconnected from power and then I try to "connect" with ST-LINK in power down mode I just get the message "No STM32 target found!"
2023-02-08 6:00 AM
Your pin list omit GND i hope connected
2023-02-08 6:07 AM
It was connected to GND, but that was actually the problem, that part of the PCB wasn't correctly connected to GND, I moved the cable to another part and it worked. Thanks!
2023-02-08 6:11 AM
on my STM32G0316-DISCO:
15:07:11 : ST-LINK SN : 0669FF3536324D5043013913
15:07:11 : ST-LINK FW : V2J39M27
15:07:11 : Board : NUCLEO-G031J6
15:07:11 : Voltage : 3.23V
15:07:11 : SWD freq : 4000 KHz
15:07:11 : Connect mode: Normal
15:07:11 : Reset mode : Hardware reset
15:07:11 : Device ID : 0x466
15:07:11 : Revision ID : Rev 1.1
15:07:11 : ST-LINK SN : 0669FF3536324D5043013913
15:07:11 : ST-LINK FW : V2J39M27
15:07:11 : Board : NUCLEO-G031J6
15:07:11 : Voltage : 3.23V
15:07:11 : SWD freq : 4000 KHz
15:07:11 : Connect mode: Normal
15:07:11 : Reset mode : Hardware reset
15:07:11 : Device ID : 0x466
15:07:11 : Revision ID : Rev 1.1
15:07:11 : Debug in Low Power mode is not supported for this device.
15:07:11 : UPLOADING OPTION BYTES DATA ...
15:07:11 : Bank : 0x00
15:07:11 : Address : 0x40022020
15:07:11 : Size : 112 Bytes
15:07:11 : UPLOADING ...
15:07:11 : Size : 1024 Bytes
15:07:11 : Address : 0x8000000
15:07:11 : Read progress:
15:07:11 : Data read successfully
15:07:11 : Time elapsed during the read operation is: 00:00:00.006
have a different firmware version, why?
Device..ID are same, so what *is* the difference?
Different voltages?
Try lowering the SWD Speed significantly.
still: "Error: Database" makes me nervous.
hth
KnarfB