cancel
Showing results for 
Search instead for 
Did you mean: 

What is the white plastic debugger connector of STM32C0316-DK?

Pavel A.
Super User

The white plastic clip on the board for ST-LINK3-MINIE debugger:

https://www.st.com/en/evaluation-tools/stm32c0316-dk.html

Is it available to order separately? For different board thickness?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
S.Ma
Principal

It is a board to board connector from Kyocera, typically used for LED strips. Spec here

It is on sale at most distributors such as RS Components and others.

This is only for standard thickness PCB. Otherwise, TAG Connect or MIPI-10/14 with ribbon can be used.

Not the same cost, not reusable.

Because of standard PCB thickness, it is also possible to solder a DF11-10DP Hirose connector which enables more permanent connector that supports cables with your chosen pinout, easier than ribbons or a bench of flying jumper wires...

View solution in original post

1 REPLY 1
S.Ma
Principal

It is a board to board connector from Kyocera, typically used for LED strips. Spec here

It is on sale at most distributors such as RS Components and others.

This is only for standard thickness PCB. Otherwise, TAG Connect or MIPI-10/14 with ribbon can be used.

Not the same cost, not reusable.

Because of standard PCB thickness, it is also possible to solder a DF11-10DP Hirose connector which enables more permanent connector that supports cables with your chosen pinout, easier than ribbons or a bench of flying jumper wires...