cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to connect and flash program to STM32F407(custom board)

Cpatt.1
Associate II

  1)is crystal is required to be used for program flashing 

2) boot0 to be low or High

Note: I'm using ST-LINK V2

2 REPLIES 2

It doesn't need an external crystal as it runs from HSI.

The BOOTx pin shouldn't make a lot of difference unless the user code sleeps the device or reconfigures pins.

M​ore likely you're not powering it properly, issues with VDDA or VCAP

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
MM..1
Chief III

How stlink you use explain SWD connection show photo...