2024-05-04 10:24 PM
I need to download the STM32F4DISCOVERY board firmware package for the MATLAB toolbox, but it's not available for download on the official website.
2024-05-05 12:01 AM - edited 2024-05-05 12:01 AM
Hello @oleehu and welcome to the ST Community :smiling_face_with_smiling_eyes:.
For such a firmware package, i suggest you to the Mathworks website.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-05-05 05:02 AM
But MathWorks doesn't provide download packages, the download link on the MathWorks website redirects to the ST official website.
2024-05-05 06:02 AM
As I recollect support for the STM32's was integrated into MatLab at some point. MIL? (Micro-processor In the Loop)
There was like one guy at ST that supported the original effort. You'd do better checking in the MatLab orientated forums, than here.