cancel
Showing results for 
Search instead for 
Did you mean: 

The STM32F4DISCOVERY board firmware package cannot be downloaded.

oleehu
Associate II

I need to download the STM32F4DISCOVERY board firmware package for the MATLAB toolbox, but it's not available for download on the official website.

3 REPLIES 3
STTwo-32
ST Employee

Hello @oleehu and welcome to the ST Community :smiling_face_with_smiling_eyes:.

For such a firmware package, i suggest you to the Mathworks website.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

But MathWorks doesn't provide download packages, the download link on the MathWorks website redirects to the ST official website.

As I recollect support for the STM32's was integrated into MatLab at some point. MIL? (Micro-processor In the Loop)

There was like one guy at ST that supported the original effort. You'd do better checking in the MatLab orientated forums, than here.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..