2023-03-16 08:23 AM
When I try too start debugging I get this message:
I checked the drivers and the device is showing as a USB Composit Device and I have no alternative to change the driver.
I installed en.stsw-link009 and successfully installed some drivers but they are not available in device manager.
I uninstalled the device in device manager but still no change.
I even installed the newest STM32CubeIDE 1.12.0 but still no change.
Does anybody have another idea?
Solved! Go to Solution.
2023-03-16 09:12 AM
Sorry, I made a mistake - the supply voltage does not route via JP1, but is connected directly to the STM32F103. So you can disconnect it again and set the jumper back to the bottom side.
The other jumpers were set correctly (PWR = U5V, IDD = set and 2 jumpers on ST-LINK).
If the USB port on your computer works otherwise, there are now only two possibilities: the USB cable is defective or the ST-LINK has been damaged.
Regards
/Peter
2023-03-16 09:15 AM
Bad cables, won't work with charging cables.
Try different cables, try different USB ports.
Avoid docking stations and hubs.
Got a multi-meter or scope, perhaps check board voltages.
2023-03-16 09:17 AM
I'll get a new cable and come back to you, Thanks for the help!
2023-03-16 04:28 PM
I tried with another cable it was still not working.
But, I changed PC to my desktop and it worked, it probably had something to do with my laptop not exactly sure what, I'm going to continue working from my desktop and hopefully it's going to work now.
The difference now is the power led is green.