2025-01-30 04:38 AM - last edited on 2025-01-30 06:35 AM by Sarra.S
Hi all
I am trying to program an STM32U575RIT6 chip using a TAG connect and ST link V3, on plugging in the tag connect, the chip shorts and becomes unrecoverable. I make sure to ground the linker before inserting, doing it all on a grounded matt, with the power to the board off before plugging it in.
This seems to happen at random, as sometimes the programming will work and program fine, other times it shorts. I replace it with a new chip and it works for a while and then shorts again. When the chip is programmed, it works fine and as expected, until the point I come to reprogram it and it shorts.
I've tried other ST links, and cables, to verify its not just my linker and still get the same results. I've tried keeping the board powered on when I plug the STM link in, and still get the issue.
I've moved from using an STM32L452 and STM32L496 which I never had any problems with programming, only ever this U5 chip.
Any advice on what I am doing wrong, or how to stop this from happening.
I've added the schematic diagram for the ST link to my chip for reference.
Thanks in advance :)
2025-01-30 06:36 AM
Hello @southernGB,
The 10µF capacitor (C71) on the SWD lines might be causing issues, try reducing the capacitance or removing it temporarily to see if the issue persists?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-01-30 08:14 AM
Hi @Sarra.S ,
I've tried this method and the STM32U5 has still shorted out when the ST link is connected.
2025-01-30 08:28 AM
Then you'll need to review the connector, and what it connects too. Make sure you've not mirrored or confused the pin designations.
This isn't a standard 10/20-pin JTAG as exported by the ST-LINK's
Review your netlist. Review all pin assignments.
Review part orientation.
Check analogue supply.
Check voltage on VCAP pin
2025-01-30 08:40 AM
PC13 probably isn't suitable for driving things, it's typically in a low-power domain
Do not put an operating board on a conductive surface or foam.
Check unpopulated board vs net-list.
2025-01-30 03:55 PM
I suspect a ground loop might be the fault. How is the board powered, how are grounds isolated?
10 uF cap on NRST is way too high. Should be 0.1 uF. I'm not sure if this will cause issues. Is VDD decoupled? Is VDDA connected to VDD? Lots of details we can't see in the portion of the schematic you sent. Consistent issues with chips shorting suggest a protection diode is getting blown. Is VDD stable? Generated from an LDO?