cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO-F429ZI Replacement

mckim0306
Associate

Hi, I am developing the board using the NUCLEO-F429ZI board CN7, CN8, CN9 and CN10 of ST, and I am looking for a product to upgrade to several surfaces such as FD CAN Port.

According to ST's data, Nucleo-H743zi seems to be compatible except NC in CN9, but according to circuit diagram data, it doesn't seem to be compatible at all.

What data should I look at and judge?

I'm sharing the data I saw.
Looking at the circuit diagram and pin map, it seems to be inconsistent.

2 REPLIES 2
mƎALLEm
ST Employee

Hello,

They are not the same board:

NUCLEO-F429ZI: MB1137

Nucleo-H743ZI: MB1364

ST tries to make a pinout compatibly as much as possible between the boards but in some cases couldn't reach 100% of it.

Now, as you are using FDCAN. PD0/PD1 are at the same place on both boards. Meanwhile the ZIO connectors seem to be compatible.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Imen.D
ST Employee

Hello @mckim0306 ,

I recommend you check and compare different part numbers and their characteristics using "Cross selector" feature within STM32CubeMX:

ImenD_0-1738578830836.png

 

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen