STM32L496ZGT6 internal regulator output voltage
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-02-06 2:01 AM
Hi
I have a problem with my board with STM32L496ZGT6.
Some boards works fine (so.. i think there isn't a project problem) some boards are in loop during the power on.
I exaplin better:
Here a function in main.cpp:
/*Configure the main internal regulator output voltage...............................................*/
if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE2) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
void _Error_Handler(char *, int)
{
while(1){}
}
If I comment:
/*Configure the main internal regulator output voltage...............................................*/
/*
if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE2) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/*.....
The board power on reguarly so it means:
HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE2) != 0
This is esay but why does this happen?
Hardware problem?
Here the function HAL_PWREx_ControlVoltageScaling:
HAL_StatusTypeDef HAL_PWREx_ControlVoltageScaling(uint32_t VoltageScaling)
{
uint32_t wait_loop_index = 0;
assert_param(IS_PWR_VOLTAGE_SCALING_RANGE(VoltageScaling));
#if defined(PWR_CR5_R1MODE)
if (VoltageScaling == PWR_REGULATOR_VOLTAGE_SCALE1_BOOST)
{
/* If current range is range 2 */
if (READ_BIT(PWR->CR1, PWR_CR1_VOS) == PWR_REGULATOR_VOLTAGE_SCALE2)
{
/* Make sure Range 1 Boost is enabled */
CLEAR_BIT(PWR->CR5, PWR_CR5_R1MODE);
/* Set Range 1 */
MODIFY_REG(PWR->CR1, PWR_CR1_VOS, PWR_REGULATOR_VOLTAGE_SCALE1);
/* Wait until VOSF is cleared */
wait_loop_index = (PWR_FLAG_SETTING_DELAY_US * (SystemCoreClock / 1000000));
while ((wait_loop_index != 0) && (HAL_IS_BIT_SET(PWR->SR2, PWR_SR2_VOSF)))
{
wait_loop_index--;
}
if (HAL_IS_BIT_SET(PWR->SR2, PWR_SR2_VOSF))
{
return HAL_TIMEOUT;
}
}
/* If current range is range 1 normal or boost mode */
else
{
/* Enable Range 1 Boost (no issue if bit already reset) */
CLEAR_BIT(PWR->CR5, PWR_CR5_R1MODE);
}
}
else if (VoltageScaling == PWR_REGULATOR_VOLTAGE_SCALE1)
{
/* If current range is range 2 */
if (READ_BIT(PWR->CR1, PWR_CR1_VOS) == PWR_REGULATOR_VOLTAGE_SCALE2)
{
/* Make sure Range 1 Boost is disabled */
SET_BIT(PWR->CR5, PWR_CR5_R1MODE);
/* Set Range 1 */
MODIFY_REG(PWR->CR1, PWR_CR1_VOS, PWR_REGULATOR_VOLTAGE_SCALE1);
/* Wait until VOSF is cleared */
wait_loop_index = (PWR_FLAG_SETTING_DELAY_US * (SystemCoreClock / 1000000));
while ((wait_loop_index != 0) && (HAL_IS_BIT_SET(PWR->SR2, PWR_SR2_VOSF)))
{
wait_loop_index--;
}
if (HAL_IS_BIT_SET(PWR->SR2, PWR_SR2_VOSF))
{
return HAL_TIMEOUT;
}
}
/* If current range is range 1 normal or boost mode */
else
{
/* Disable Range 1 Boost (no issue if bit already set) */
SET_BIT(PWR->CR5, PWR_CR5_R1MODE);
}
}
else
{
/* Set Range 2 */
MODIFY_REG(PWR->CR1, PWR_CR1_VOS, PWR_REGULATOR_VOLTAGE_SCALE2);
/* No need to wait for VOSF to be cleared for this transition */
/* PWR_CR5_R1MODE bit setting has no effect in Range 2 */
}
#else
/* If Set Range 1 */
if (VoltageScaling == PWR_REGULATOR_VOLTAGE_SCALE1)
{
if (READ_BIT(PWR->CR1, PWR_CR1_VOS) != PWR_REGULATOR_VOLTAGE_SCALE1)
{
/* Set Range 1 */
MODIFY_REG(PWR->CR1, PWR_CR1_VOS, PWR_REGULATOR_VOLTAGE_SCALE1);
/* Wait until VOSF is cleared */
wait_loop_index = (PWR_FLAG_SETTING_DELAY_US * (SystemCoreClock / 1000000));
while ((wait_loop_index != 0) && (HAL_IS_BIT_SET(PWR->SR2, PWR_SR2_VOSF)))
{
wait_loop_index--;
}
if (HAL_IS_BIT_SET(PWR->SR2, PWR_SR2_VOSF))
{
return HAL_TIMEOUT;
}
}
}
else
{
if (READ_BIT(PWR->CR1, PWR_CR1_VOS) != PWR_REGULATOR_VOLTAGE_SCALE2)
{
/* Set Range 2 */
MODIFY_REG(PWR->CR1, PWR_CR1_VOS, PWR_REGULATOR_VOLTAGE_SCALE2);
/* No need to wait for VOSF to be cleared for this transition */
}
}
#endif
return HAL_OK;
}
Any advice?
Solved! Go to Solution.
- Labels:
-
STM32L4 series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-02-06 2:50 AM - edited ‎2024-02-06 2:55 AM
Hello,
According to the RM, the dafault PWR config after reset is VOS1:
And there is a sequence to switch from VOS1 to VOS2:
Also what is your system frequency? You can't exceed 26MHz at VOS2!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-02-06 2:42 AM - edited ‎2024-02-06 3:00 AM
@AndrewFFFF wrote:Some boards works fine (so.. i think there isn't a project problem)
That's not an entirely safe assumption: it could be that the design is marginal - so some boards just work, while others just fail ...
The PWR_REGULATOR_VOLTAGE_SCALE2 has a number of limitations - are you sure you are strictly within them all?
A complex system designed from scratch never works and cannot be patched up to make it work.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-02-06 2:50 AM - edited ‎2024-02-06 2:55 AM
Hello,
According to the RM, the dafault PWR config after reset is VOS1:
And there is a sequence to switch from VOS1 to VOS2:
Also what is your system frequency? You can't exceed 26MHz at VOS2!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-02-06 3:17 AM
Thank you for your fast answers:
I "inherited" this board and i didn't project this board, so i need time to replay your question.
Here in main.cpp:
#if USE_20_MHZ_CLOCK
//For 20Mhz core clock freq
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV4;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
#endif
#if USE_40_MHZ_CLOCK
//For 40Mhz core clock freq
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV2;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV8;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
#endif
I think 40_MHz for debug mode
About the hardware i share some photo about the power supply:
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-02-06 3:22 AM
I've already said: you need to implement the sequence to switch from VOS1 to VOS2.
To me it's not a HW issue for the moment. You need to implement the sequence as described in the RM.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-02-06 3:25 AM
@AndrewFFFF wrote:
#if USE_20_MHZ_CLOCK
//For 20Mhz core clock freq
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV4;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
#endif
#if USE_40_MHZ_CLOCK
//For 40Mhz core clock freq
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV2;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV8;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
#endif
I think 40_MHz for debug mode
As already noted, you can't run at 40MHz with VOS2 - Therefore this code
/*Configure the main internal regulator output voltage*/
if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE2) != HAL_OK)
needs to check that you are in the USE_20MHZ_CLOCK mode ...
A complex system designed from scratch never works and cannot be patched up to make it work.