STM32L432KC communication with microSD card Reader via SPI
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-08-04 12:37 PM
I am following this video: https://www.youtube.com/watch?v=aqSNz26Cuio&t=35s
Hardware:
- STM32 Nucleo-32 for STM32L432
- Adafruit microSDcard adapter: https://www.adafruit.com/product/4682
- Samsung 32GB EVO (red) microSD card
Software:
- STM32CubeIDE
The board used in the video is different but all the settings are also present in my STM32L432 board.
My .ioc pinout view looks like this:
Note: In video, the SPI1_SCK has been automatically given to PA5, but for my board it was shown as PA1, hence have made the connections accordingly.
FatFS enabled:
- MAX_SS - 4096
- USE_LFN - Enabled with static working buffer
SPI1 enabled:
- Mode - Full Duplex - Master
- Parameter Settings -
- System Core SYS set to Serial Wire (as shown in video)
After following the video, My build is complete with no errors. Then I make the hardware connections for my board like this:
(Please excuse the microSD card not inserted in the slot)
When I am running the file to download the code to board, I am changing the run config file as shown in the video: changing the debug probe to OpenOCD (I don't know much about what this does) and changing the Reset mode to Software System Reset.
So when I click on Run, I get the following error:
Open On-Chip Debugger 0.11.0+dev-00449-g53fa0f7 (2022-06-09-09:42) [https://github.com/STMicroelectronics/OpenOCD]
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : STLINK V2J40M27 (API v2) VID:PID 0483:374B
Info : Target voltage: 3.265263
Info : Unable to match requested speed 8000 kHz, using 4000 kHz
Info : Unable to match requested speed 8000 kHz, using 4000 kHz
Info : clock speed 4000 kHz
Info : stlink_dap_op_connect(connect)
Info : SWD DPIDR 0x2ba01477
Info : STM32L432KCUx.cpu: Cortex-M4 r0p1 processor detected
Info : STM32L432KCUx.cpu: target has 6 breakpoints, 4 watchpoints
Info : starting gdb server for STM32L432KCUx.cpu on 3333
Info : Listening on port 3333 for gdb connections
Info : accepting 'gdb' connection on tcp/3333
Info : device idcode = 0x10016435 (STM32L43/L44xx - Rev Z : 0x1001)
Info : RDP level 0 (0xAA)
Info : flash size = 256kbytes
Info : flash mode : single-bank
Warn : GDB connection 1 on target STM32L432KCUx.cpu not halted
undefined debug reason 8 - target needs reset
Info : accepting 'gdb' connection on tcp/3333
Warn : GDB connection 2 on target STM32L432KCUx.cpu not halted
undefined debug reason 8 - target needs reset
target halted due to debug-request, current mode: Thread
xPSR: 0x01000000 pc: 0x08000e9c msp: 0x20010000
Info : Unable to match requested speed 8000 kHz, using 4000 kHz
Info : Unable to match requested speed 8000 kHz, using 4000 kHz
Info : Padding image section 0 at 0x08006304 with 4 bytes (bank write end alignment)
target halted due to debug-request, current mode: Thread
xPSR: 0x01000000 pc: 0x08000e9c msp: 0x20010000
Info : dropped 'gdb' connection
target halted due to debug-request, current mode: Thread
xPSR: 0x21000000 pc: 0x08000fc4 msp: 0x2000ffdc
shutdown command invoked
Info : dropped 'gdb' connection
When I run using the default setting in Run Config; which is debug probe set to ST-LINK (ST-LINK GDB server), I get no errors while downloading to board, but I don't see any file written on to the SD card. Attaching the console log of the same below:
STMicroelectronics ST-LINK GDB server. Version 7.0.0
Copyright (c) 2022, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.11.0
-------------------------------------------------------------------
Log output file: C:\Users\RSL\AppData\Local\Temp\STM32CubeProgrammer_a17636.log
ST-LINK SN : 066BFF525649898367212344
ST-LINK FW : V2J40M27
Board : NUCLEO-L432KC
Voltage : 3.27V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x435
Revision ID : Rev Z
Device name : STM32L43xxx/STM32L44xxx
Flash size : 256 KBytes
Device type : MCU
Device CPU : Cortex-M4
BL Version : --
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a17636.srec
File : ST-LINK_GDB_server_a17636.srec
Size : 24.75 KB
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 12]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:00.960
Verifying ...
Download verified successfully
Shutting down...
Exit.
I am fairly new to the whole STM32 environment.
I just want to make this STM32L432 + SPI + microSDcard thing working.
Any help is appreciated. Thank you.
Solved! Go to Solution.
- Labels:
-
SPI
-
ST-Link
-
STM32CubeIDE
-
STM32L4 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-08-04 01:09 PM
SD Cards would want 512-byte sectors.
I don't use CubeMX/IDE to code.
There should be mostly working code for SPI + FATFS here
STM32Cube_FW_L4_V1.14.0\Drivers\BSP\Adafruit_Shield\stm32_adafruit_sd.c
There were some bugs with the multi-sector support that I've addressed previously on the forum, but good luck finding them, search here is an abomination..
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-08-04 01:09 PM
SD Cards would want 512-byte sectors.
I don't use CubeMX/IDE to code.
There should be mostly working code for SPI + FATFS here
STM32Cube_FW_L4_V1.14.0\Drivers\BSP\Adafruit_Shield\stm32_adafruit_sd.c
There were some bugs with the multi-sector support that I've addressed previously on the forum, but good luck finding them, search here is an abomination..
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-08-10 11:53 AM
Thank you very much for the solution. I am looking at the library you just mentioned past couple of days. Will keep working on it.
Let's see. Thank you again.