2024-09-26 4:11 AM
I downloaded the boot code generated by following the settings in Figure 3 (the frequency configuration to 600Mhz) into the flash of the 0x08000000 starting address, and then the stlink cannot detect after re-powering (as shown in Figure 1). But my device manager can detect the device (as shown in Figure 2).
Can someone help me with that? Thank you very much!
figure1
figure2
figure3
Solved! Go to Solution.
2024-10-10 3:11 AM - edited 2024-10-11 12:43 AM
Hello @Gaobo and welcome to the community;
Could you please
I hope this help you!
Please let me know if the issue is solved or not?
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-10-10 3:11 AM - edited 2024-10-11 12:43 AM
Hello @Gaobo and welcome to the community;
Could you please
I hope this help you!
Please let me know if the issue is solved or not?
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-10-11 6:45 PM
Thank you very much!