cancel
Showing results for 
Search instead for 
Did you mean: 

stm32h753 NUCLEO board manual not have details about CN2 dfu connector

yogui_ricardo
Associate II

stm32h753 nucleo manual not have details about CN2 dfu connector

1 ACCEPTED SOLUTION

Accepted Solutions
SofLit
ST Employee

Hello @yogui_ricardo ,

CN2 is dedicated to connect to the MCU (STM32F723) that manages STLINK-V3 and update its firmware over SWD:

PA13: SWDIO

PA14: SWCLK

SofLit_0-1730231982437.png

But I don't think user needs this connection as the firmware could be updated over ST-LINK micro USB connector (CN1) using STM32CubeProgrammer or ST-LINK firmware upgrade tool.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Imen.D
ST Employee

Hello @yogui_ricardo and welcome to the Community,

Which detail are you looking for ?

Maybe the Gerber files can help you. For that, you can look at the Board Manufacturing specifications in the CAD resources.

NUCLEO-H753ZI - STM32 Nucleo-144 development board with STM32H753ZI MCU, supports Arduino, ST Zio and morpho connectivity - STMicroelectronics

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
SofLit
ST Employee

Hello @yogui_ricardo ,

CN2 is dedicated to connect to the MCU (STM32F723) that manages STLINK-V3 and update its firmware over SWD:

PA13: SWDIO

PA14: SWCLK

SofLit_0-1730231982437.png

But I don't think user needs this connection as the firmware could be updated over ST-LINK micro USB connector (CN1) using STM32CubeProgrammer or ST-LINK firmware upgrade tool.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.