cancel
Showing results for 
Search instead for 
Did you mean: 

stm32h753 NUCLEO board manual not have details about CN2 dfu connector

yogui_ricardo
Associate II

stm32h753 nucleo manual not have details about CN2 dfu connector

1 ACCEPTED SOLUTION

Accepted Solutions
SofLit
ST Employee

Hello @yogui_ricardo ,

CN2 is dedicated to connect to the MCU (STM32F723) that manages STLINK-V3 and update its firmware over SWD:

PA13: SWDIO

PA14: SWCLK

SofLit_0-1730231982437.png

But I don't think user needs this connection as the firmware could be updated over ST-LINK micro USB connector (CN1) using STM32CubeProgrammer or ST-LINK firmware upgrade tool.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: Be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.

View solution in original post

2 REPLIES 2
Imen.D
ST Employee

Hello @yogui_ricardo and welcome to the Community,

Which detail are you looking for ?

Maybe the Gerber files can help you. For that, you can look at the Board Manufacturing specifications in the CAD resources.

NUCLEO-H753ZI - STM32 Nucleo-144 development board with STM32H753ZI MCU, supports Arduino, ST Zio and morpho connectivity - STMicroelectronics

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
SofLit
ST Employee

Hello @yogui_ricardo ,

CN2 is dedicated to connect to the MCU (STM32F723) that manages STLINK-V3 and update its firmware over SWD:

PA13: SWDIO

PA14: SWCLK

SofLit_0-1730231982437.png

But I don't think user needs this connection as the firmware could be updated over ST-LINK micro USB connector (CN1) using STM32CubeProgrammer or ST-LINK firmware upgrade tool.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: Be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.