2024-02-08 4:44 AM
Hi ST Support Team,
I am Using STM32H743XIH6 in one of the project.
Having Query related to crystal frequency.
In datasheet frequency characteristics is provided for oscillator input.
In my Design and STM32H743XIH6 Evaluation Board crystal is implemented.
My Design contains 48Mhz Crystal while EVM contains 25Mhz crystal.
Kindly go through the attached schematic capture of developed board waveform capture at PH0-OSC_IN pin.
Getting same waveform as per Evaluation Kit (Find Attached EVM waveform)
Hope waveform we observed will specify the MCU clock requirement in terms of rise time, fall time, VIH & VIL level.
want to make sure that there is no issue in MCU Clock using external 48 Mhz crystal implementation.
in 25 Mhz & 48 Mhz crystal maximum amplitude is going at 1.8V and MCU operating at 3.3V level.
Hoping that the clock at OSC_PIN is satisfying MCU operating level.
Thanks,
2024-02-08 4:54 AM
Check the datasheet, for H733 its is:
6.3.9 External clock source characteristics
High-speed external user clock generated from an external source
fHSE_ext User external clock source frequency max 50 MHz
2024-02-08 5:09 AM
Hi LCE,
After Referring the H733, 6.3.9.
Found, maximum Low Level of Clock need to be 0.3*VDD (= 0.7*3.3 = 0.99), in my case & in EVM it is ~1.2V
For Minimum High Level of clock need to be 0.7*VDD (= 0.7 *3.3 = 2.31), in my case & in EVM it is ~1.8V.
So considering datasheet parameter for both board not maintaining required level, correct?
Can you help me to get resolution on above concern?
Thanks..
2024-02-08 5:12 AM
Max external crystal frequency is 48 MHz, which yours meets. You should have load capacitors loaded.
The waveform looks fine.
See here for crystal selection design guide:
2024-02-08 5:29 AM
2024-02-08 5:32 AM
Hi
Find attached snap, ignore previous one..
Thanks,
2024-02-08 6:29 AM
I imagine the capacitance of your scope is distorting things as well.
> Crystal having 8 pF load capacitance, added 8 pF capacitor at both pins and getting same result as without load capacitance.
Just because it works doesn't mean it will continue to do so. Follow the recommendations to have the best chance of success. A little surprised it's working at all without any load caps.
Don't mix up specifications for the external clock input with specifications for the external crystal.
2024-02-08 6:34 AM
Hi TDK,
We kept Load Capacitance Open due to STM32 10pF Load capacitance.
STM32 Capacitance matching Load capacitance requirement for crystal.
Thanks,
2024-02-08 8:51 AM
> STM32 10pF Load capacitance.
Where are you getting this from?
The required load caps on a CL=8pF crystal should be about 2 * 8 pF - 6 pF = 10pF.
2024-02-08 7:40 PM
Hi TDK,
Referring to attached snap considering STM32 10pF load capacitance.
Thanks,