cancel
Showing results for 
Search instead for 
Did you mean: 

HAL_DSI_Init() stuck on error

Ricko
Senior III

Hi,

the application gets stuck on the Error_Handler() in the piece of code below in main.c

 

 

  hdsi.Instance = DSI;
  hdsi.Init.AutomaticClockLaneControl = DSI_AUTO_CLK_LANE_CTRL_DISABLE;
  hdsi.Init.TXEscapeCkdiv = 4;
  hdsi.Init.NumberOfLanes = DSI_TWO_DATA_LANES;
  hdsi.Init.PHYFrequencyRange = DSI_DPHY_FRANGE_80MHZ_100MHZ;
  hdsi.Init.PHYLowPowerOffset = PHY_LP_OFFSSET_0_CLKP;
  PLLInit.PLLNDIV = 32;
  PLLInit.PLLIDF = DSI_PLL_IN_DIV1;
  PLLInit.PLLODF = DSI_PLL_OUT_DIV2;
  PLLInit.PLLVCORange = DSI_DPHY_VCO_FRANGE_500MHZ_800MHZ;
  PLLInit.PLLChargePump = DSI_PLL_CHARGE_PUMP_2000HZ_4400HZ;
  PLLInit.PLLTuning = DSI_PLL_LOOP_FILTER_2000HZ_4400HZ;
  if (HAL_DSI_Init(&hdsi, &PLLInit) != HAL_OK)
  {
    Error_Handler();
  }

 

 

I just noticed that DSI lane clock is set to 32MHz - screenshot below - from the HSE (8MHz crystal) which seems too low. To what frequency (in the clock diagram page) do I set the two DSI clocks (DSI TXCLKESC and DSI lane byte clock)? How is that calculated?

 

There is no return value for the function Error_Handler() so in debug mode there I cannot check the return value by hovering the mouse pointer over it. How can I see the return value of that function so I can see what the error code is?

 

Attached is the .IOC file with the current DSI settings if it helps.

 

Thank you :)

Rick

Ricko_1-1741496086965.png

Ricko_2-1741496396470.png

 

Ricko_0-1741496058160.png

 

 

 

0 REPLIES 0