2025-02-02 11:28 PM - last edited on 2025-02-03 02:54 AM by Andrew Neil
STM32H735G-DK debug Question
I try to use board STM32H735G-DK.
I connected JP7 to the STLK to change the power source and connected the PC and board via CN15 with USB microB.
In STM32CubeIDE 1.13.0, I make project for the board and debug ( Fig.1 ).
I haven't added anything to the created files, but debugging failed ( Fig.2 ).
The state of the board is
・the monitor is white screen
・LD1 and LD2 is not light
・LD5 is green and LD6 is red
Fig. 1
Fig. 2
I thought it might be a deadlock state, so I tried to recover from the deadlock using the STM32CubeProgrammer method as described in the documentation ( https://www.st.com/resource/en/user_manual/um2679-discovery-kit-with-stm32h735ig-mcu-stmicroelectronics.pdf 6.2.4).
When I debug after running the method, I get Figure 3 in the debug console. If I debug again I get back to Figure 2.
What was wrong with my settings?
Could you please give me some advice on how to restore the state and perform debugging?
Fig. 3
Solved! Go to Solution.
2025-02-03 02:19 AM - edited 2025-02-03 02:19 AM
Hello,
Most probably the behavior is related to an already raised issue in CubeMx in this thread.
Go to the preprocessor in your IDE and remove the USE_PWR_LDO_SUPPLY definition:
2025-02-02 11:44 PM
Hello @HO_MR and welcome to the ST Community.
I suggest you to Check this article. It should be helpful. Also, i suggest you to update to use the Last version of the STM32CubeIDE (V1.17.0).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-02-03 01:09 AM
Thank you for your reply @STTwo-32.
I have updated ST32CubeIDE.
I read the article you shared and did the following three things:
- Checked PA13 (SWDIO) and PA14 (SWCLK). Fig
- Executed ST32CubeProgrammer with the settings in the article
- Set the debug configuration with the settings in the article
But after debugging, I ended up in the same state as in the question.
What else should I be suspicious of?
2025-02-03 02:19 AM - edited 2025-02-03 02:19 AM
Hello,
Most probably the behavior is related to an already raised issue in CubeMx in this thread.
Go to the preprocessor in your IDE and remove the USE_PWR_LDO_SUPPLY definition:
2025-02-03 05:13 PM
Thank you for your reply, @SofLit.
I really appreciate your support. I also understand the community rules.
Thank you again.