2024-05-10 04:47 AM - edited 2024-05-10 04:48 AM
Hello,
I want to develop logger with flash drive and STM32H753 (NUCLEO-H753) using STM32Cube. I started to develop this application with USB_OTG_FS (which is soldered on this board) - successfully completed. Then I wanted to change to USB_OTG_HS. This peripheral is not soldered on the nucleo, so I made my own connector (according to the nucleo connection - USB A connector with ESD protection) and connect it with the nucleo.
If I run the firmware (generated by stm32cube)it still calls the USBH_UserProcess callback when the USB drive is connected. The id value changes between HOST_USER_CONNECTION and HOST_USER_UNRECOVERED_ERROR (HOST_USER_CONNECTION, HOST_USER_UNRECOVERED_ERROR, HOST_USER_CONNECTION... and so on).
Does anyone know how to fix this issue?
Thank you for your response.
Solved! Go to Solution.
2024-05-10 06:15 AM
This happens when the D+ and D- pins are swapped.
2024-05-10 06:15 AM
This happens when the D+ and D- pins are swapped.
2025-01-18 10:27 PM
Hello, I am a first-year graduate student at Shandong University of Technology. I am currently using l9663. Can you provide me with some example programs? Even just a function for writing data to the l9663 register will do. I want to test whether there is a problem with my board.If possible, I would really appreciate it.