STM32H7 base schematic review
- January 17, 2025
- 1 reply
- 1177 views
I have attached herewith the first iteration of the schematic for my custom stm32 board utilizing the H753ZIT6 MCU.
I would like to clear few doubts regarding
1) In the nucleo schematic for the same, STM has used F7 MCU for their ST Link interface, should I do the same? or rely on SWD/JTAG for boot and programming.
2) I am evaluating between choosing either JTAG or SWD for my main means of communicating with the IC, should I make provision for both of these on a single connector?
3) If I am choosing not buy the STLINK V3 or V2, what do I need to take care of, from both a hardware and software point of view?
4) The oscillators chosen are: TSX-3225_24.0000MF20G-AC0 for HSE and CM8V-T1A-32.768k-9pF-20PPM-TB-QA for LSE. Is their respective circuitry correct and in general the chosen oscillators right? I read the AN2867 guide but most of the recommended oscillators were over-budget for my specific project.
This is my first time ever being involved in hardware design, so if any common mistake is found, please let me know.
Thank You