2019-07-29 6:13 AM
What exactly is the difference between Nucleo boards Nucleo-F303RE, Nucleo-F411RE and Nucleo-F446RE? To me, the data brief seems to suggest that they are the same. Can someone point out the difference? Is it okay if I buy any of these according to the availability? Have attached the Date brief for reference.
Solved! Go to Solution.
2019-08-15 7:29 AM
Hi @skrowten_hermit ,
You need to refer to UM1724.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2019-07-29 6:29 AM
FLASH, RAM and SPEED?
F3 has different ADC performance.
You should probably look up the webpages for the micro-controller placed on each board.
If all that is unimportant for your unspecified application, any of them would suffice.
2019-07-29 9:04 PM
As stated above, there are speed & core ram/flash differences but also additional/different peripherals: CAN, UARTS, I2S, SPI (count), USB (type), etc...
There are nice pictorials of the boards over on the mbed.org website (color breakout of features on board) that might make it easier to understand
https://os.mbed.com/platforms/ST-Nucleo-F446RE/
2019-07-31 10:38 PM
This helps. I was looking for something like this. Thank you!
2019-08-15 7:29 AM
Hi @skrowten_hermit ,
You need to refer to UM1724.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.