2023-04-13 12:00 PM
When connecting a brand new STM32F3348-DISCO board to USB on my MacBook Pro (M1, Ventura), USB communication fails and the ST-Link is not recognised. LD2 flashes brightly red and LD1 flashes hardly visible.
Sometimes the communication works for a very short moment. Updating the ST-Link firmware is not possible since USB communication fails.
Is this a known issue and what can I do?
2023-04-18 12:02 PM
Final attempt...
Tried the board on a Windows machine. Same result. The Nucleo board starts up flawless and gets recognised as a functioning USB device in the system settings. With the same cable the disco board does not work and the USB driver in system settings gives an error.
Conclusion: I have to scrap the board
2023-04-18 02:34 PM
Okay, so it's a hummmm... :\
What puzzles me most is, that - as you've said - the demo works with a charge-only cable, yet does not work with charger plus the full cable...
I understand your frustration. Pity the world is not smaller so that we could discuss it personally...
JW
2023-04-18 10:17 PM
Hypothesis:
If USB data is corrupted, STLink halts the Disco board. If data is not corrupted (e.g. no data) the STLink starts the Disco board.
No frustration. I work in the industry and know that the world is not perfect ;)
Thanks for your responses JW.
Greetings,
P@