2022-05-25 05:31 AM
Hello I am trying to move a small io project to smaller chip. I am trying no code project just confirm enter debugger works.
STM32F103C8T6
STM32Cube IDE 1.9
I Get ST-Link Error When attempting to debug. Reason(18) Could not verify ST device! Abort connection.
Error halting cpu. See attached. Any suggestions?
Open On-Chip Debugger 0.11.0+dev-00443-gcf12591 (2022-02-09-13:33) [ST Internal]
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : STLINK V2J39S7 (API v2) VID:PID 0483:3748
Info : Target voltage: 3.280321
Info : Unable to match requested speed 8000 kHz, using 4000 kHz
Info : Unable to match requested speed 8000 kHz, using 4000 kHz
Info : clock speed 4000 kHz
Info : stlink_dap_op_connect(connect)
Info : SWD DPIDR 0x2ba01477
Info : STM32F103C8Tx.cpu: Cortex-M3 r2p0 processor detected
Info : STM32F103C8Tx.cpu: target has 6 breakpoints, 4 watchpoints
Info : starting gdb server for STM32F103C8Tx.cpu on 3333
Info : Listening on port 3333 for gdb connections
Info : STM32F103C8Tx.cpu: external reset detected
Info : accepting 'gdb' connection on tcp/3333
target halted due to debug-request, current mode: Thread
xPSR: 0x01000000 pc: 0x080000f0 msp: 0x20002800
Info : Unable to match requested speed 8000 kHz, using 4000 kHz
Info : Unable to match requested speed 8000 kHz, using 4000 kHz
Info : device id = 0x10010414
Info : flash size = 256kbytes
O.K.
O.K.:0xE00FFFD0
Info : dropped 'gdb' connection
shutdown command invoked
2022-10-10 01:12 AM
This might be out of topic since I'm using PlatformIO and Arduino but I managed to upload and debug a clone. Maybe the configuration bellow can help someone:
[env:STM32F103C8_CLONE]
platform = ststm32
board = genericSTM32F103C8
framework = arduino # arduino, mbed, cmsis, ...
debug_tool = stlink
upload_protocol = stlink # stlink , dfu
build_flags = -Wl,--undefined,_printf_float
upload_flags = -c set CPUTAPID 0x2ba01477 # Working upload for clone
debug_server =
~/.platformio/packages/tool-openocd/bin/openocd
-s ~/.platformio/packages/tool-openocd/scripts
-f interface/stlink.cfg
-c "transport select hla_swd"
-c "set CPUTAPID 0x2ba01477" # Working debug for clone
-f target/stm32f1x.cfg
-c "reset_config none"