STM32F103C8T6 Debugging
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-05-25 5:31 AM
Hello I am trying to move a small io project to smaller chip. I am trying no code project just confirm enter debugger works.
STM32F103C8T6
STM32Cube IDE 1.9
I Get ST-Link Error When attempting to debug. Reason(18) Could not verify ST device! Abort connection.
Error halting cpu. See attached. Any suggestions?
Open On-Chip Debugger 0.11.0+dev-00443-gcf12591 (2022-02-09-13:33) [ST Internal]
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : STLINK V2J39S7 (API v2) VID:PID 0483:3748
Info : Target voltage: 3.280321
Info : Unable to match requested speed 8000 kHz, using 4000 kHz
Info : Unable to match requested speed 8000 kHz, using 4000 kHz
Info : clock speed 4000 kHz
Info : stlink_dap_op_connect(connect)
Info : SWD DPIDR 0x2ba01477
Info : STM32F103C8Tx.cpu: Cortex-M3 r2p0 processor detected
Info : STM32F103C8Tx.cpu: target has 6 breakpoints, 4 watchpoints
Info : starting gdb server for STM32F103C8Tx.cpu on 3333
Info : Listening on port 3333 for gdb connections
Info : STM32F103C8Tx.cpu: external reset detected
Info : accepting 'gdb' connection on tcp/3333
target halted due to debug-request, current mode: Thread
xPSR: 0x01000000 pc: 0x080000f0 msp: 0x20002800
Info : Unable to match requested speed 8000 kHz, using 4000 kHz
Info : Unable to match requested speed 8000 kHz, using 4000 kHz
Info : device id = 0x10010414
Info : flash size = 256kbytes
O.K.
O.K.:0xE00FFFD0
Info : dropped 'gdb' connection
shutdown command invoked
- Labels:
-
ST-Link
-
STM32F1 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-05-25 5:38 AM
Board has counterfeit MCU on it.
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
2022-05-25 5:43 AM
Yes, as @Community member mentioned, this again looks very much like a fake STM32, because the original STM32F103C8T6 has 64KB flash and reports ID 0x410, while yours reports 256KB flash and ID 0x414. No wonder that the STM32CubeIDE does not want to work with it.
Already wrote in another thread with exactly the same issue:
Unfortunately, the massive current demand, which has been impossible to satisfy for some time, is calling for counterfeiters with fakes on a large scale. They are found particularly often, for example, on the Blue Pill boards popular with beginners. Sometimes the fakes can be recognised by the markings used on the package, but sometimes they can only be recognised by details.
So if you mean the STM32 that is on the BluePill in your photo, then it is almost certainly a fake.
Regards
/Peter
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-05-25 5:45 AM
This is NOT an STM32F103 MCU, so the STLink refuses to talk to it. Real STM32 has an id of 0x1ba01477. You will not be able to debug it using the current version of ST-Link. You may either downgrade to the old version or use another BluePill with the proper firmware as CMSIS-DAP interface for debugging (but not from STM32CubeIDE).
Your MCU will execute the STM32F103 firmware programmed into it but ST tools don't support it since the are made to support only microcontrollers made by STM, not the clones.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-05-25 5:58 AM
Oh thanks for the info. The label make it look quite real.
Is there some way to make sure I get a real chip next time?
Like should I order directly from ST or something?
I guess I could swap out the chips or something.
For the time being did you say there is some older version of STLink that supports these fake ones until I can find some real ones? I have been using a STm32f4-discovery from st up until now. I would like to use a smaller package for a small io project though so It thought I would move to this chip because there was so much info on internet about it. I like using the STM32CubeIDE so I would like to continue to use it. if possible.
I would imagine that open ocd could possibly be modified or slightly different chip used but it would like you said not align with the original project.
I understand if you do not want to help support random chips with official ST stuff like STM32CubeIDE so that would be fine too. Perhaps I could ask open OCD for slight mod or something like that for these 10 dev boards i got.
Then when I make my boards I can order chips directly from ST or something like that to make sure I get real ones?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-05-25 6:23 AM
To be honest I got 10 of the cheap boards because there was a good canbus tutorial online that used that board, I ported it to the STM32F4 and it worked so I was like ohh good, and I am making a small 10 node simple can setup to test some software and stuff for future use so I was like i will order some of those blue pill boards from the example with the STM32F103C8T6
The funny thing is I already have STM32F103C8T6 chip on the STm32F4-disovery board as the debugger circuit.....I noticed the STM32F1 has one can bus interface and smaller io count and is cheaper than the STM32F4 on the Discovery board so I thought I would try that for example a simple stand alone push button / gpio canbus device or an analog knob on canbus type thing. I just want to play around with a can network and get the feel for what is possible that type of thing.
The nucleo line looks good....but the example i ran into was blue pill so I was more inclined to do that..it was funny to me that the neucleo basically has a bluepill on there as the debugger...lol...or should I say the blue pill is a copy of that debugger circuit.
If I cannot get this batch to work with STM32CubeIDE or find a good debugger for these or a good source of these chips perhaps I should order 10 nucleos or something like that for small can bus test setup before making my own boards. and go with the nucleo chips STM32L432KC I think those are lower powered so that is nice. is there a good canbus example for the nucleo 32 I think that would be a good option as well.
I just see the STM32F103C8T6 all over the place so it makes me more comfortable to proceed with that one.
Perhaps We should keep this on topic here though. Should I contact Open OCD to see if this chip can be added to some extra unofficial setting that can be used in STM32CubeIDE for the time being or should I consider these chips not valid for the 10 can node test setup using SMT32CubeIDE and try to order some more and hope they have good chips on them lol.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-05-25 6:40 AM
I ported this
https://www.youtube.com/watch?v=JfWlIY0zAIc
To my STM32F4 and it worked. So I was like 10 blue pills please for multi node test...lol...now stuck.
Probably would have gone nucleo if there was a comparable nucleo 32 example. I would prefer the lower powered device. ;) oooooooh welll..... again is see the STM32F103C8T6 everywhere...like every board with an stlink built onto it...the maple dev board...the blue pills...I think they are all copies of the stlink v2 scematic lol...ohhhh welll...
I think it would be entertaining to fix the compiler for the random ones I got but I am not sure if that is official or if I should even put it on here or over at the ocd forum now so as not to annoy st themselves into supporting other peoples products...I am still a little confused as to how the label ended up so official looking though lol.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-05-25 7:11 AM
@JLall.2 "Is there some way to make sure I get a real chip next time?"
I don't think there's any 100% foolproof way - even famous names have been caught out; eg, https://blog.adafruit.com/2011/08/11/counterfeit-parts-are-a-big-headache/
The main thing is to only buy from reputable sources - which probably, sadly, rules out the BluePill. :\
A complex system designed from scratch never works and cannot be patched up to make it work.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-05-27 8:55 PM
Well I think that answers that question. I cant find another F1 board with the small package, usb portl and crystal populated at the moment so I will probably try and order some STM32F103C8T6 from the st link to digi key and swap them out and see how that goes. Thanks for the help. I see another forum post where someone looks to have success with that so it sounds like I am in a similar situation and will try that route when I get some time.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-05-27 8:59 PM
I can only flash these by jumping the boot pins and sending data over a usb to ttl uart adapter like this example here. Obviously that does not allow for debugging though so I will try and order some genuine chips for that.
https://circuitdigest.com/microcontroller-projects/programming-stm32f103c8-board-using-usb-port
I would imagine I could also setup open ocd to use the other chips but I think that is for another forum since these are not ST parts so I will leave that discussion for some other place. Thanks again for the help.