2019-12-05 12:56 AM
I freshly installed STM32CubeIDE (with J-LINK and ST-LINK selected during install) and created a new projekt. When trying to create a debug configuration Segger J-LINK is not selectable as debug adapter - only ST-Link.
Tried on Windows and Linux.
Also tried to install Segger JLINK tools afterwards with no effect.
Best,
P
Solved! Go to Solution.
2019-12-05 02:17 AM
It's fixed internally and will be part of the next release.
2019-12-05 01:03 AM
Hi, there was an answer from an ST employe not too long ago. Apperently, because of H7 dual core mcu's the J-Link option has been taken out for H7. I just had a look and It is still present for F7 etc.
2019-12-05 02:03 AM
OK - I'm using an STM32H7 indeed .. but a single-core version.
Would be great if JLINK support was added for these MCUs.
2019-12-05 02:17 AM
It's fixed internally and will be part of the next release.
2020-01-10 01:21 AM
Solved if STM32CubeIDE 1.2.0 release according to me