cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE 1.1.0 does not offer Segger J-LINK debug probe in debug configurations

peter__
Associate II

I freshly installed STM32CubeIDE (with J-LINK and ST-LINK selected during install) and created a new projekt. When trying to create a debug configuration Segger J-LINK is not selectable as debug adapter - only ST-Link.

Tried on Windows and Linux.

Also tried to install Segger JLINK tools afterwards with no effect.

Best,

P

1 ACCEPTED SOLUTION

Accepted Solutions

It's fixed internally and will be part of the next release.

View solution in original post

4 REPLIES 4
hansd56
Senior II

Hi, there was an answer from an ST employe not too long ago. Apperently, because of H7 dual core mcu's the J-Link option has been taken out for H7. I just had a look and It is still present for F7 etc.

peter__
Associate II

OK - I'm using an STM32H7 indeed .. but a single-core version.

Would be great if JLINK support was added for these MCUs.

It's fixed internally and will be part of the next release.

Cartu38 OpenDev
Lead II

Solved if STM32CubeIDE 1.2.0 release according to me