2024-12-09 7:11 AM
How does one connect the STLink debug port to an older target with 0.025 square posts on 2.54 mm ptch for the debug connections? As best I can tell, the supplied cables only support 1.27 mm pitch,
Solved! Go to Solution.
2024-12-10 10:35 PM
I finally got around to using my STLINK-V3PWR or trying. The issue is lack of thought on STM side, one simple adapter like all those ARM adapters but with a 10 pin 1.27mm pitch connector instead of the 2.0mm pitch they have. I purchased the V3PWR since it has a type C connector instead of the micro USB connector and all the power stuff my standalone power board does but with a case. I think I'll have to make a cable, after hunting for several hours I see no solutions. I had one of these https://bit.ly/4g6lPst laying around, with some soldering and crimping it's a start. A real solution would be a bundle like this https://bit.ly/3D9dA0l with a 1.27mm pitch 10 pin instead of the 2mm pitch 10 pin connector.
2024-12-11 12:47 AM
Please provide direct links - URL shorteners pose a security/privacy risk:
https://www.kaspersky.co.uk/blog/link-shorteners-privacy-security/26422/
2024-12-11 3:54 AM - edited 2024-12-11 4:56 AM
Thank you, Kevin. I too purchased the device without paying close attention to the connecting cable. Shame on me as I worked this same issue in another job with TI processors/debuggers. It is sad that without the adapter I will make, the promise of good power profiling and correlation with the running firmware is lost.
I will have to cobble up to solve it, or engineer my own board.
Pictured is a legacy board.
Clyde
2025-01-06 10:05 AM - edited 2025-01-07 7:50 AM
So, I made one...
Seems like it should have been included in the box.